P2041 boot from Nor flash CS0 timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2041 boot from Nor flash CS0 timing

1,861件の閲覧回数
wxwangyan
Contributor I

  I am having a p2041 processor card.

i have set the hard corded rcw value of scr_rcw_cfg 11000 16 bit nor flash now, So P2041 will work at 600MHz platform,LCLK0 will be 18.75MHz I captured the waveform for CS0 from P2041. The CS0 signal's active "0" level time is about 110ns when boot up from nor flash, the same as signal LGPL2.

 Chapter 13 Enhanced Local Bus Controller, Table 13-16. Reset value of OR0 Register ,  The GPCM value of OR0 will be 

0000_0FF7, so that The CS0 signal's active "0" level time will be tCSRP=(1+2*SCY) ,16* LCLK0 will be about 0.85us.

But i measured the timing of CS0 boot time is 110ns, pls help to resolve it? 

0 件の賞賛
返信
2 返答(返信)

1,752件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please verify pull-up on pin L2 "LGPL4/LGTA/LUPWAIT/LPBSE" is this pull-up is present, properly mounted and has desired value.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,752件の閲覧回数
wxwangyan
Contributor I

attached waveform of CS0 from P2041cs0_2.pngcs0_1.png

0 件の賞賛
返信