P2041 RDB SATA problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2041 RDB SATA problems

ソリューションへジャンプ
4,474件の閲覧回数
sinanakman
Senior Contributor III

We received our P2041RDB sometimes ago but could never have SATA working. During boot up here is message we are receiving :

ata1: Hardreset failed, not on-lined                                      
ata1: reset failed (errno=-5), retrying in 10 secs                        
ata2: Hardreset failed, not on-lined                                      
ata2: reset failed (errno=-5), retrying in 10 secs                        
ata1: Hardreset failed, not on-lined                                      
ata1: reset failed (errno=-5), retrying in 35 secs                        
ata2: Hardreset failed, not on-lined                                      
ata2: reset failed (errno=-5), retrying in 35 secs                        
ata1: limiting SATA link speed to 1.5 Gbps                                
ata2: limiting SATA link speed to 1.5 Gbps                                
ata2: Hardreset failed, not on-lined                                      
ata2: reset failed, giving up                                             
ata1: Hardreset failed, not on-lined                                      

ata1: reset failed, giving up

We didn't change any of the settings as the box arrived.

Is there anything that needs to be modified to have the SATA disk working ?

Regards

Sinan Akman

ラベル(1)
タグ(1)
1 解決策
3,729件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

This is caused by the board configuration RCW problem, the default RCW in the shipped P2041RDB is rcw_14g_1500mhz.bin which doesn't support SATA. Please use RCW RR_PH_0x19/rcw_5g_1500mhz.bin which includes SerDes protocol 0x19 to configure the board to use SATA.

You could find RCW images in the prebuilt images ISO, and flash RCW in the alternate bank on P2041RDB.

元の投稿で解決策を見る

8 返答(返信)
3,730件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

This is caused by the board configuration RCW problem, the default RCW in the shipped P2041RDB is rcw_14g_1500mhz.bin which doesn't support SATA. Please use RCW RR_PH_0x19/rcw_5g_1500mhz.bin which includes SerDes protocol 0x19 to configure the board to use SATA.

You could find RCW images in the prebuilt images ISO, and flash RCW in the alternate bank on P2041RDB.

3,729件の閲覧回数
连营张
Contributor I

my board is also p2041RDB.

0 件の賞賛
返信
3,729件の閲覧回数
连营张
Contributor I

hi,Yiping Wang.my question is the same as Sinan Akman's.But when i update the RCW(RR_PH_0x19/rcw_5g_1500mhz.bin)to support SATA,i just can't boot from bank1.What causes it?Looking forward to your reply.

0 件の賞賛
返信
3,729件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello lianying,

Please create a separate thread to describe your problem in more details, do you use NOR Flash boot, do you update images in the alternate bank? Please provide u-boot log and your operating steps.

Thanks,

Yiping

0 件の賞賛
返信
3,729件の閲覧回数
gopikrishnan
Contributor III

Hi Yipping,

While using command "cpld reset altbank" and normal boot - both shows message as below, hence experiencing the same problem even after changing RCW file.

"Board: P2041RDB, CPLD version: 4.1 vBank: 1"

I would like to boot from alternate bank, Could you give the the hardware switch settings to boot from alternate bank.

Thanks & Reg,

Gopi Krishnan S

0 件の賞賛
返信
3,729件の閲覧回数
addiyi
NXP Employee
NXP Employee

SW2[2] is the switch that set the NOR flash bank:

Select NOR flash bank

OFF: Bank0 is used for booting

ON: Bank1 is used for booting

Adrian

0 件の賞賛
返信
3,729件の閲覧回数
sinanakman
Senior Contributor III

Hi Yiping, thanks much for your reply. I will give this a try and let you know.  Is RCW RR_PH_0x19/rcw_5g_1500mhz.bin file available somewhere else other than the CD. I am now in another location. Can I download the ISO ?


Thanks

Sinan Akman

0 件の賞賛
返信
3,729件の閲覧回数
sinanakman
Senior Contributor III

Hi Yipping, just tested rcw_5g_1500mhz.bin and seems to enable SATA. Thanks

Sinan Akman

0 件の賞賛
返信