P2040: Problem with setup eTSEC1 as GPIO output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2040: Problem with setup eTSEC1 as GPIO output

1,084件の閲覧回数
andreykondraten
Contributor I

I have a problem with using eTSEC1 signal group as a GPIO30, GPIO31.

It retains "0" on this pins (EC1_TXD1/GPIO[30] , EC1_TXD3/GPIO[31]).

RCW seems to be right (RCW[2C]: F8 DA 4E F6), it was generated by "Configuration Suite".

Other functions (ex. SDRAM, SDHC, NAND, ...) and other GPIO working good.

Reason was: two RCW fields for one purpose. To activate GPIO 30-31, both RCW 352-353, 360-361 fields to be properly setted (0b11, 0b01). Last one has unobvious description "01: 1588 and external timestamping functionality."

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)