P2020DS assembly error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020DS assembly error

4,544 Views
pierre-antoinem
Contributor III

Hi,

In my P2020 project i'm using assembly code the same way I was using it on a P5020 board.

The problem is that i'm getting these kind of errors.

"expected a inline assembler directive"

for this exemple in a .c file:

__asm__ __volatile__( "instruction ;"

                                   : [outputs]

                                   : [inputs]

                                   : [clobered list] };

and

"Instructions must occur within code section"

for this exemple in a .asm file :

.global myFunction

myFunction:

    lis 3, 0x0001

    ori 3, 3, 0x0001

    mtspr 1010, 3

    blr

If any one can help resolving these errors, it would be very nice.

Thanks.

Labels (1)
0 Kudos
Reply
10 Replies

4,149 Views
pierre-antoinem
Contributor III

Went for a solution with both macro's and functions.

Not exactly what I expected to do but it's acceptable.

Thanks for those who tried to help.

Problem solved.

0 Kudos
Reply

4,149 Views
scottwood
NXP Employee
NXP Employee

Could you show the actual asm statement?  I'm assuming it doesn't literally say [outputs] etc., and can't tell whether closing brace rather than parentheses is in your actual source code or not.  Also clarify what sort of compiler you're using.

As for the asm file, what section are you trying to place that in?  Are there any section directives earlier in the file?

0 Kudos
Reply

4,149 Views
pierre-antoinem
Contributor III

The code shown is for example.

it would be like this (example that works for gcc on p5020):

__asm__ __volatile__(

                                  "lis 3, 0x0001;"

                                  "ori 3, 3, 0x0001;"

                                  "mtspr 1010, 3;"

                                   :

                                   :

                                   : "3" };

I'm using the default tool chain for P2020. (in CW in doesn't indicate what kind of compiler it uses so I was a litle bit lost)

As i'm porting some code from a P5020 I'd prefer use a GCC compiler.

I guess changing the tool chain for a gcc version should be good ?

0 Kudos
Reply

4,149 Views
pierre-antoinem
Contributor III

I used the asm{} format instead of the asm( "instruction;" : outputs : inputs : clobered list);

C variables can be called directly with there names

And in .asm files I need to specify

.section . text

which wasn't needed for the P5020 compiler

The PA\PA_Support\Templates\Sources\P2020\Common examples where helpfull

Thanks to Marius.

Other problem :

With this compiler includes seem not to work...

I mean for example: #include "test.h"

I get Link Failed

And some Undefined functions  (that are in test.h)

Is there a documentation for this compiler ?

0 Kudos
Reply

4,149 Views
marius_grigoras
NXP Employee
NXP Employee

You should include the folder with your headers in User Recursive Path (take a look in the below picture) from -> right click on your project -> Properties -> C/C++ build -> PowerPC Compiler -> Input -> User recursive path

include.png

0 Kudos
Reply

4,149 Views
pierre-antoinem
Contributor III

I still have the same errors.

I have a directory where all my .c .h .asm files are included in user path.

Is it possible to set the equivalent default P5020's compiler (PowerPC AEABI e5500 C Compiler) to the P2020 ?

If yes, how can I do it ?

0 Kudos
Reply

4,149 Views
marius_grigoras
NXP Employee
NXP Employee

Can you share the project or show us a more detailed log?

About the compiler, the answer is a negative one. The aeabi gcc compiler for e5500 core cannot be used for e500v2 (P2020). Officially, we don't have "gcc" support for P2020 processor, but if you want to use a "gcc toolchain" instead, you can make a P1021RDB selecting 'GCC EABI e500v2' and just copy/replace your P2020 files into the project. This trick should work without issues.

Regards,

Marius

0 Kudos
Reply

4,149 Views
pierre-antoinem
Contributor III

Sorry, but i'm can't show the code.

The main problem was the compiler not accepting my code.

I used the syntax given in the examples linked. (using "inline" for some functions was causing that problem)

I have a last question :

I'm my inline assembly function how can I call an assembler macro located in a .asm file.

i'm using #include "myMacroFile.asm"

but I get this error : "expected inline assembler directive" for  "myMacroName:"  ".macro"   ".endm"

0 Kudos
Reply

4,149 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

I guess that you're using CodeWarrior for PA? In positive case, please pay attention that P5020 is gcc based and P2020 is MW FSL based (a different compiler). You can take a look in this folder

PA\PA_Support\Templates\Sources\P2020\Common for eppc_exception.asm and interrupt.c to see some asm routins for P2020.

Regards,

Marius

4,149 Views
scottwood
NXP Employee
NXP Employee

Hmm?  You certainly can use GCC and Linux with P2020.

0 Kudos
Reply