P2020 how much FLOPS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 how much FLOPS

2,297件の閲覧回数
smiletan
Contributor I

I am ready to use P2020.My application want strong float point processing capacity  bigger than 13GPLOPS.Is the chip P2020 OK for my app?

0 件の賞賛
返信
2 返答(返信)

2,235件の閲覧回数
smiletan
Contributor I

Thanks.

Then IMX6Q float point processing capacity ? Can I use IMX6Q to suit for 13GFLOPS?

0 件の賞賛
返信

2,235件の閲覧回数
ufedor
NXP Employee
NXP Employee

> My application want strong float point processing capacity bigger than 13GPLOPS.

> Is the chip P2020 OK for my app?

No.

P2020 has e500v2 cores executing floating-point arithmetic instructions, except for divide, with 1-cycle throughput.

For two cores at 1333 MHz this could give 2.6 GFLOPs

0 件の賞賛
返信