P2020 Power On Reset Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 Power On Reset Configuration

1,355 Views
mdz
Contributor I

Are the Vil max/Vih min thresholds for the power on reset configuration pins the same as regular logic levels? For example, if the RGMII interface is set up to operate at 2.5V, does a power on reset config pin using an RGMII pin have 2.5V CMOS thresholds?

0 Kudos
Reply
1 Reply

1,186 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes the Vil max/Vih min thresholds for the power on reset configuration pins are the same as regular logic levels. For example, if the RGMII interface is set up to operate at 2.5V, a power on reset config pin using an RGMII pin have 2.5V CMOS thresholds.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply