P2020 - Power Consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 - Power Consumption

1,470 Views
michaelkachalov
Contributor I

Hello,

I am looking at the P2020EC datasheet rev 2 08/2013, dual e500 core device. The data listed in Table 5 (under section 2.3) 'P2020 Core Power Consumption,' is that for a single core or for both cores? That is, a maximum power dissipation of 6.1W at core frequency 800MHz is listed. Would the total consumption of both cores be 6.1W or 12.2W?

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,275 Views
alexander_yakov
NXP Employee
NXP Employee

This is for both cores. For single core version please look datasheet for P2010, this document contains less values.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply