P2010 eSDHC, different commands SD spec <> P2010 spec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2010 eSDHC, different commands SD spec <> P2010 spec

1,519 Views
michalszlachetk
Contributor I

Hello,

im using P2010 and eSDHC, but i found some differences between SD Card spec and P2010 spec (check https://www.sdcard.org/downloads/pls/ -> Simplified , cmd20, cmd26, cmd27) are used for something completely different than in P2010 manual. Could you explain this a little bit?

Best Regards

Michal Szlachetka

Labels (1)
Tags (3)
3 Replies

1,235 Views
Pavel
NXP Employee
NXP Employee

I can see that P2010 use part of possibility for CMD20.

SDHC Specification contains information that CMD26 is reserved.

 

It looks like that you should not use CMD26 in your code.

Have a great day,
Pavel Chubakov

1,235 Views
Pavel
NXP Employee
NXP Employee

There is little difference for CMD20 only.

Is there problem for using these commands on your board?

Have a great day,
Pavel Chubakov

0 Kudos
Reply

1,235 Views
michalszlachetk
Contributor I

Thanks for your reply Pavel :smileyhappy:

At this moment not, but i don't know how it will be when i port code to another uC (which is possible and SD protocol usage should be the same regardless of uC -> only very low level implementation should be changed)

Br

Michal

0 Kudos
Reply