P1025RDB hypervisor support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1025RDB hypervisor support.

1,462 Views
ramakirankumar
Contributor I

Hi,

I have a QorIQ p1025rdb eval board with me. I have taken the sdk 1.2 where the board is supported and have the setup ready, with uboot.

There is an HV in the tmp/deploy/images folder of the yocto release dir. But i could not located the HV DTB, as told in the support document chapter 4.2.1.8 for Hypervisor Deployment.

Does P1025RDB is supported for nxp hypervisor ?

If so could  you let me know how to configure the uboot to load the hypervisor and where can i locate the dtb ?

Regards,

Ram

Labels (1)
0 Kudos
Reply
1 Reply

1,393 Views
scottwood
NXP Employee
NXP Employee

The embedded hypervisor is not supported on P1025 or any other e500v2-based SoC.  KVM is supported, though.

Also note that SDK 1.2 is very old.  I recommend using a recent upstream kernel instead, especially if you want to use KVM.

0 Kudos
Reply