P1022 flash programming production tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1022 flash programming production tools

2,303 Views
michelots
Contributor I

We have an application using the P1022NXE2LFB and a Micron PC28F256M29EWHX flash and currently we're looking for an easy to use and economic flash programming solution suitable for a production environment. For sporadic programming we use the CodeWarrior USB TAP and CodeWarrior IDE but this is not suitable for production use. Suggestions for a proper solution are more than welcome.

Labels (1)
0 Kudos
Reply
4 Replies

2,101 Views
michelots
Contributor I

Hello Alexander,

Thanks for your prompt reply. Any third-party hardware and software you can recommend with a production environment in mind?

Regards,

Michel

0 Kudos
Reply

2,101 Views
sinanakman
Senior Contributor III

Hi Michel

I saw this a bit late. Some of our customers are using

bdiPro for production. Here is the link :

bdiPro - Abatron AG 

Hope this helps

Regards

Sinan Akman

0 Kudos
Reply

2,101 Views
jimccall
Contributor I

Hi Michael,

We're using a similar Micron flash device for our custom board. I was wondering what flash algorithm you were using to program the flash. Any information would be great, thanks!

Sincerely,

Jesse

0 Kudos
Reply

2,101 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, there are no other flash programmer tools available from NXP for this processor, we offer only CodeWarrior.

Please consider using third-party tools.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply