P1021 cache-inhibited?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1021 cache-inhibited?

1,800 Views
zwilcox
Contributor IV

I'm working with the P1021.  The Reference Manual states that if CCSR space is used, then it should be marked as cache-inhibited and guard.

pastedImage_1.png

How do I mark this address space, or any other address space as cache-inhibited and guarded?

Labels (1)
0 Kudos
Reply
2 Replies

1,631 Views
ufedor
NXP Employee
NXP Employee

Corresponding MMU TLB has to have I and G bits set - please refer to the PowerPC™ e500 Core Family Reference Manual, 12.3.6 TLB Entry Field Definitions:

https://www.nxp.com/docs/en/reference-manual/E500CORERM.pdf 

1,631 Views
zwilcox
Contributor IV

Thank you sir.

0 Kudos
Reply