P1021 Large page NAND flashinng using Code warrior.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1021 Large page NAND flashinng using Code warrior.

ソリューションへジャンプ
1,703件の閲覧回数
safeerkt
Contributor II

Hello,

We have a custom design based on P1021MDS.In our initial design, we were having a small page flash device which is 512Mb. We have upgraded the NAND device with a large page Micron device which is having 1Gb. We were not able to flash the new NAND before and we have changed some FCM related register in the config file. After this, it started flashing but the boot prints are not coming. It will be really appreciated if someone can share some thoughts on this.

Many Thanks,

Safeer

ラベル(1)
0 件の賞賛
返信
1 解決策
1,572件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is required to check the NAND Flash datasheet section "Error Management" to ensure that the device is supported by the FCM which is capable to correct only 1-bit error in a 512-byte data block.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,573件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is required to check the NAND Flash datasheet section "Error Management" to ensure that the device is supported by the FCM which is capable to correct only 1-bit error in a 512-byte data block.

0 件の賞賛
返信