P1011: Multiple PCIe Controllers and Modes?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1011: Multiple PCIe Controllers and Modes?

1,867 Views
stevebelvin
Contributor I

Can the P1011 be configured to operate two separate PCI Express controllers at the same time over separate x1 connections?  If so, can these two controllers be in different device modes at the same time?  That is, can one be configured as a RC on its port while the other is an EP on its port?

Labels (1)
0 Kudos
Reply
2 Replies

1,687 Views
ufedor
NXP Employee
NXP Employee

> can one be configured as a RC on its port while the other is an EP on its port?

This configuration is possible.

Please refer to the P1020 QorIQ Integrated Processor Reference Manual, 4.5.3.5 Host/agent configuration and 4.5.3.6 I/O port selection.

0 Kudos
Reply

1,687 Views
stevebelvin
Contributor I

Thank you for the reference to the power-up config options for the PCIe interfaces.

0 Kudos
Reply