P1010RDB LEDs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1010RDB LEDs

1,803件の閲覧回数
jamiefinney
Contributor I

Good afternoon,

I am new to the P1010 and the RDB.  Are there any usable LEDs on the board that can be actuated from early boot, say in the bootrom?

Jamie

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,689件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Are you trying to flashing LEDs by yourself from early boot? I have checked the P1010RDBPBUG.pdf Rev.0, and did not find one usable for the purpose, so I am afraid no. Correct me if this is not your meaning.

0 件の賞賛
返信

1,689件の閲覧回数
catalindemergia
Contributor IV

Hi,

I found this code in u-boot\arch\powerpc\lib\board.c

#if defined(CONFIG_STATUS_LED) && defined(STATUS_LED_BOOT)

    status_led_set(STATUS_LED_BOOT, STATUS_LED_BLINKING);

#endif

This seems to do what you want I don't see a flag used so that this will be executed only

for one processor, this code is used for the all processors from the PowerPC family. The

CONFIG_STATUS_LED flag is used to enable the blinking feature in particular.

Maybe this can be a starting point for you,

Catalin

0 件の賞賛
返信