P1010 booting from SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010 booting from SPI

2,358 Views
tsybezoff
Contributor II

Hi to all!

Please, help me)

I can't understand how to boot my project code into SPI Flash.

As I know, I need to create a configuration file and my user code image. How can I do this using Code Warrior IDE?)

Labels (1)
Tags (3)
2 Replies

1,761 Views
roybieda
NXP Employee
NXP Employee

Have you had a chance to look at this Application Note?: http://www.freescale.com/files/32bit/doc/app_note/AN3659.pdf


0 Kudos
Reply

1,761 Views
lunminliang
NXP Employee
NXP Employee

Some related information can be found in Targeting_PA_Processors.pdf, section 6.1 Working With Flash Programmer and appendix C Memory Configuration Files. The document is in the CodeWarrior installation directory, C:\Program Files\Freescale\CW PA v10.x\PA\Help\PDF.

0 Kudos
Reply