P1010 booting from SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1010 booting from SPI

1,805 次查看
tsybezoff
Contributor II

Hi to all!

Please, help me)

I can't understand how to boot my project code into SPI Flash.

As I know, I need to create a configuration file and my user code image. How can I do this using Code Warrior IDE?)

标签 (1)
标记 (3)
2 回复数

1,208 次查看
roybieda
NXP Employee
NXP Employee

Have you had a chance to look at this Application Note?: http://www.freescale.com/files/32bit/doc/app_note/AN3659.pdf


0 项奖励
回复

1,208 次查看
lunminliang
NXP Employee
NXP Employee

Some related information can be found in Targeting_PA_Processors.pdf, section 6.1 Working With Flash Programmer and appendix C Memory Configuration Files. The document is in the CodeWarrior installation directory, C:\Program Files\Freescale\CW PA v10.x\PA\Help\PDF.

0 项奖励
回复