P1010 booting from SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1010 booting from SPI

2,398件の閲覧回数
tsybezoff
Contributor I

Hi to all!

Please, help me)

I can't understand how to boot my project code into SPI Flash.

As I know, I need to create a configuration file and my user code image. How can I do this using Code Warrior IDE?)

ラベル(1)
タグ(3)
2 返答(返信)

1,801件の閲覧回数
roybieda
NXP Employee
NXP Employee

Have you had a chance to look at this Application Note?: http://www.freescale.com/files/32bit/doc/app_note/AN3659.pdf


0 件の賞賛
返信

1,801件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Some related information can be found in Targeting_PA_Processors.pdf, section 6.1 Working With Flash Programmer and appendix C Memory Configuration Files. The document is in the CodeWarrior installation directory, C:\Program Files\Freescale\CW PA v10.x\PA\Help\PDF.

0 件の賞賛
返信