P1010-RDB won't boot from norflash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010-RDB won't boot from norflash

Jump to solution
1,527 Views
s0m31
Contributor I

I can't get it to boot from norflash but it boots up fine from nandflash.

I set the switches on my board to the following to get it to boot from the norflash but my console doesn't show anything.

The switches are set to the following:

SW4[1-4]: 1111

SW6[4]: 0

From what I can gather from the documentation, it is possible that SW6[4] is overridden by I2C1.

Am I missing something or is it due to I2C1?

Labels (1)
0 Kudos
Reply
1 Solution
1,325 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sothavy,

For P1010RDB-PA

• SW4[1:4] = 1111 and SW6[4] = 0 for 16-bit NOR Flash boot.

• SW4[1:4] = 1011 and SW6[4] = 0 for 8-bit NOR Flash boot.

• u-boot start address of default bank is 0xeff80000.

• u-boot start address of alternate bank is 0xeef80000

You could use the following command to switch from NAND to NOR boot.

=> i2c dev 0

=> i2c mw 18 1 f1

=> i2c mw 18 3 f0

=> mw.b ffb00011 0

=> mw.b ffb00014 2

=> mw.b ffb00015 5

=> mw.b ffb00016 3

=> mw.b ffb00017 f

=> reset

For P1010RDB-PB

SW4[1:4]= 1111 and SW3[3:4]= 00 for NOR boot


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,326 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sothavy,

For P1010RDB-PA

• SW4[1:4] = 1111 and SW6[4] = 0 for 16-bit NOR Flash boot.

• SW4[1:4] = 1011 and SW6[4] = 0 for 8-bit NOR Flash boot.

• u-boot start address of default bank is 0xeff80000.

• u-boot start address of alternate bank is 0xeef80000

You could use the following command to switch from NAND to NOR boot.

=> i2c dev 0

=> i2c mw 18 1 f1

=> i2c mw 18 3 f0

=> mw.b ffb00011 0

=> mw.b ffb00014 2

=> mw.b ffb00015 5

=> mw.b ffb00016 3

=> mw.b ffb00017 f

=> reset

For P1010RDB-PB

SW4[1:4]= 1111 and SW3[3:4]= 00 for NOR boot


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply