NOR issue after kernel booted up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NOR issue after kernel booted up

3,081件の閲覧回数
nareshpuli
Contributor III

hi,

My board is booted up from NOR Flash, After booting kernel it will shows JFFS2 issue continuously shows  like below attachemnt , i reloded the NOR Flash same issue existing how can i fix this it ?? i am trying erase nor flash using codwarrior but it flash id error, not connecting, please help its stopping my work.

p2020rdb login: root

after kernel boot up below statements are coming in terminal  continuously, i am not able to control how can i come out of thsi problem, please help me

issue

[JFFS2 DBG] (2176) ver_insert: Link new node at c7617bd4 (root is c7617bd4)
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: Add ef53b9d8 (v 3, 0x2000-0x3000, ov 0) to fragtree
[JFFS2 DBG] (2176) jffs2_add_full_dnode_to_inode: adding node 0x2000-0x3000 @0x001cb854 on flash, newfrag *ef5f8978
[JFFS2 DBG] (2176) ver_insert: Link new node at c7617bd4 (root is c7617bd4)
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: Add ef53b5a0 (v 2, 0x1000-0x2000, ov 0) to fragtree
[JFFS2 DBG] (2176) jffs2_add_full_dnode_to_inode: adding node 0x1000-0x2000 @0x001caf78 on flash, newfrag *ef5f8990
[JFFS2 DBG] (2176) ver_insert: Link new node at c7617bd4 (root is c7617bd4)
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: Add ef53bbe0 (v 1, 0x0-0x1000, ov 0) to fragtree
[JFFS2 DBG] (2176) jffs2_add_full_dnode_to_inode: adding node 0x00-0x1000 @0x001caaac on flash, newfrag *ef5f89a8
[JFFS2 DBG] (2176) jffs2_truncate_fragtree: truncating fragtree to 0x0000ec90 bytes
[JFFS2 DBG] (2019) jffs2_truncate_fragtree: truncating fragtree to 0x00000377 bytes
[JFFS2 DBG] (2019) jffs2_kill_fragtree: killing
[JFFS2 DBG] (2176) jffs2_do_read_inode: read inode #194
[JFFS2 DBG] (2176) jffs2_do_read_inode_internal: ino #194 pino/nlink is 1
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: ino #194
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: read 40 bytes at 0x28b1e8(2).
[JFFS2 DBG] (2176) read_more: read more 28 bytes
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: insert fragment 0x2000-0x2ab0, ver 3 at 0028b1e8
[JFFS2 DBG] (2176) jffs2_lookup_tn: root c7617c18, offset 8192
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: read 40 bytes at 0x28a9cc(3).
[JFFS2 DBG] (2176) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_do_read_inode_internal: ino #216 pino/nlink is 5
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: ino #216
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x2b7bc8(2).
[JFFS2 DBG] (2019) jffs2_add_fd_to_list: add dirent "sysinfo", ino #597
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x2b7b00(2).
[JFFS2 DBG] (2019) jffs2_add_fd_to_list: add dirent "platform", ino #596
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x28d730(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) read_dnode: the node has no data.
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x00-0x00, ver 1 at 0028d730
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: keep new mdata with ver 1
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: nodes of inode #216 were read, the highest version is 595, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: potential mdata is ver 1 at ef53b5a0
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: insert fragment 0x1000-0x2000, ver 2 at 0028a9cc
[JFFS2 DBG] (2019) jffs2_do_read_inode_internal: ino #218 pino/nlink is 1
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: ino #218
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x28d824(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x00-0x0f, ver 1 at 0028d824
[JFFS2 DBG] (2019) jffs2_lookup_tn: root c733dce8, offset 0
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: nodes of inode #218 were read, the highest version is 1, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: tn ef53b5a0 ver 1 range 0x0-0xf ov 0
[JFFS2 DBG] (2019) ver_insert: Link new node at c733dd04 (root is c733dd04)
[JFFS2 DBG] (2019) check_tn_node: check node 0x00-0x0f, phys offs 0x28d824
[JFFS2 DBG] (2019) check_node_data: check node at 0x28d824, data length 15, partial CRC 0x000000, correct CRC 0x3f29cb8f, data starts at 0x28d8.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: Add ef53b5a0 (v 1, 0x0-0xf, ov 0) to fragtree
[JFFS2 DBG] (2019) jffs2_add_full_dnode_to_inode: adding node 0x00-0x0f @0x0028d824 on flash, newfrag *ef5f8858
[JFFS2 DBG] (2019) jffs2_truncate_fragtree: truncating fragtree to 0x0000000f bytes
[JFFS2 DBG] (2019) jffs2_kill_fragtree: killing
[JFFS2 DBG] (2176) jffs2_lookup_tn: root c7617c18, offset 4096
[JFFS2 DBG] (2019) jffs2_do_read_inode_internal: ino #219 pino/nlink is 1
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: ino #219
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x28d8ac(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x00-0x696, ver 1 at 0028d8ac
[JFFS2 DBG] (2019) jffs2_lookup_tn: root c733dce8, offset 0
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: nodes of inode #219 were read, the highest version is 1, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: tn ef53b5a0 ver 1 range 0x0-0x696 ov 0
[JFFS2 DBG] (2019) ver_insert: Link new node at c733dd04 (root is c733dd04)
[JFFS2 DBG] (2019) check_tn_node: check node 0x00-0x696, phys offs 0x28d8ac
[JFFS2 DBG] (2019) check_node_data: check node at 0x28d8ac, data length 761, partial CRC 0x000000, correct CRC 0xd2b5f058, data starts at 0x28d.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: Add ef53b5a0 (v 1, 0x0-0x696, ov 0) to fragtree
[JFFS2 DBG] (2019) jffs2_add_full_dnode_to_inode: adding node 0x00-0x696 @0x0028d8ac on flash, newfrag *ef5f8858
[JFFS2 DBG] (2019) jffs2_truncate_fragtree: truncating fragtree to 0x00000696 bytes
[JFFS2 DBG] (2019) jffs2_kill_fragtree: killing
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: 'this' found 0x2000-0x2ab0 (data)
[JFFS2 DBG] (2019) jffs2_do_read_inode_internal: ino #220 pino/nlink is 5
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: ino #220
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x2b8488(2).
[JFFS2 DBG] (2019) jffs2_add_fd_to_list: add dirent "sensors.conf", ino #606
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x28dc20(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) read_dnode: the node has no data.
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x00-0x00, ver 1 at 0028dc20
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: keep new mdata with ver 1
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: nodes of inode #220 were read, the highest version is 604, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: potential mdata is ver 1 at ef53b5a0
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: Ponder this ver 3, 0x2000-0xab0
[JFFS2 DBG] (2019) jffs2_do_read_inode_internal: ino #221 pino/nlink is 1
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: ino #221
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x28e570(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x2000-0x27cf, ver 3 at 0028e570
[JFFS2 DBG] (2019) jffs2_lookup_tn: root c733dce8, offset 8192
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x28e158(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x1000-0x2000, ver 2 at 0028e158
[JFFS2 DBG] (2019) jffs2_lookup_tn: root c733dce8, offset 4096
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: 'this' found 0x2000-0x27cf (data)
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: Ponder this ver 3, 0x2000-0x7cf
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x28dc9c(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x00-0x1000, ver 1 at 0028dc9c
[JFFS2 DBG] (2019) jffs2_lookup_tn: root c733dce8, offset 0
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: 'this' found 0x1000-0x2000 (data)
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: Ponder this ver 2, 0x1000-0x1000
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: nodes of inode #221 were read, the highest version is 3, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: tn ef53b5a0 ver 3 range 0x2000-0x27cf ov 0
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: tn ef53b9d8 ver 2 range 0x1000-0x2000 ov 0
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: tn ef53be60 ver 1 range 0x0-0x1000 ov 0
[JFFS2 DBG] (2019) ver_insert: Link new node at c733dd04 (root is c733dd04)
[JFFS2 DBG] (2019) check_tn_node: check node 0x2000-0x27cf, phys offs 0x28e570
[JFFS2 DBG] (2019) check_node_data: check node at 0x28e570, data length 484, partial CRC 0x000000, correct CRC 0x9b59f60d, data starts at 0x28e.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: Add ef53b5a0 (v 3, 0x2000-0x27cf, ov 0) to fragtree
[JFFS2 DBG] (2019) jffs2_add_full_dnode_to_inode: adding node 0x2000-0x27cf @0x0028e570 on flash, newfrag *ef5f8858
[JFFS2 DBG] (2019) ver_insert: Link new node at c733dd04 (root is c733dd04)
[JFFS2 DBG] (2019) check_tn_node: check node 0x1000-0x2000, phys offs 0x28e158
[JFFS2 DBG] (2019) check_node_data: check node at 0x28e158, data length 979, partial CRC 0x000000, correct CRC 0x6940ac74, data starts at 0x28d.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: Add ef53b9d8 (v 2, 0x1000-0x2000, ov 0) to fragtree
[JFFS2 DBG] (2019) jffs2_add_full_dnode_to_inode: adding node 0x1000-0x2000 @0x0028e158 on flash, newfrag *ef5f89d8
[JFFS2 DBG] (2019) ver_insert: Link new node at c733dd04 (root is c733dd04)
[JFFS2 DBG] (2019) check_tn_node: check node 0x00-0x1000, phys offs 0x28dc9c
[JFFS2 DBG] (2019) check_node_data: check node at 0x28dc9c, data length 1141, partial CRC 0x000000, correct CRC 0x6baded15, data starts at 0x28.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: Add ef53be60 (v 1, 0x0-0x1000, ov 0) to fragtree
[JFFS2 DBG] (2019) jffs2_add_full_dnode_to_inode: adding node 0x00-0x1000 @0x0028dc9c on flash, newfrag *ef5f89f0
[JFFS2 DBG] (2019) jffs2_truncate_fragtree: truncating fragtree to 0x000027cf bytes
[JFFS2 DBG] (2019) jffs2_kill_fragtree: killing
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: read 40 bytes at 0x28a234(2).
[JFFS2 DBG] (2176) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_do_read_inode_internal: ino #223 pino/nlink is 1
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: insert fragment 0x00-0x1000, ver 1 at 0028a234
[JFFS2 DBG] (2176) jffs2_lookup_tn: root c7617c18, offset 0
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: 'this' found 0x1000-0x2000 (data)
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: Ponder this ver 2, 0x1000-0x1000
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: nodes of inode #194 were read, the highest version is 3, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: tn ef53bbe0 ver 3 range 0x2000-0x2ab0 ov 0
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: tn ef31f960 ver 2 range 0x1000-0x2000 ov 0
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: tn ef53be60 ver 1 range 0x0-0x1000 ov 0
[JFFS2 DBG] (2176) ver_insert: Link new node at c7617c34 (root is c7617c34)
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: Add ef53bbe0 (v 3, 0x2000-0x2ab0, ov 0) to fragtree
[JFFS2 DBG] (2176) jffs2_add_full_dnode_to_inode: adding node 0x2000-0x2ab0 @0x0028b1e8 on flash, newfrag *ef5f89d8
[JFFS2 DBG] (2176) ver_insert: Link new node at c7617c34 (root is c7617c34)
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: Add ef31f960 (v 2, 0x1000-0x2000, ov 0) to fragtree
[JFFS2 DBG] (2176) jffs2_add_full_dnode_to_inode: adding node 0x1000-0x2000 @0x0028a9cc on flash, newfrag *ef5f89f0
[JFFS2 DBG] (2176) ver_insert: Link new node at c7617c34 (root is c7617c34)
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: Add ef53be60 (v 1, 0x0-0x1000, ov 0) to fragtree
[JFFS2 DBG] (2176) jffs2_add_full_dnode_to_inode: adding node 0x00-0x1000 @0x0028a234 on flash, newfrag *ef5f89c0
[JFFS2 DBG] (2176) jffs2_truncate_fragtree: truncating fragtree to 0x00002ab0 bytes
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: ino #223
[JFFS2 DBG] (2176) jffs2_do_read_inode: read inode #219
[JFFS2 DBG] (2176) jffs2_do_read_inode_internal: ino #219 pino/nlink is 1
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: ino #219
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: read 40 bytes at 0x28d8ac(2).
[JFFS2 DBG] (2176) read_more: read more 28 bytes
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: insert fragment 0x00-0x696, ver 1 at 0028d8ac
[JFFS2 DBG] (2176) jffs2_lookup_tn: root c7617c18, offset 0
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: nodes of inode #219 were read, the highest version is 1, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: tn ef53be60 ver 1 range 0x0-0x696 ov 0
[JFFS2 DBG] (2176) ver_insert: Link new node at c7617c34 (root is c7617c34)
[JFFS2 DBG] (2176) jffs2_build_inode_fragtree: Add ef53be60 (v 1, 0x0-0x696, ov 0) to fragtree
[JFFS2 DBG] (2176) jffs2_add_full_dnode_to_inode: adding node 0x00-0x696 @0x0028d8ac on flash, newfrag *ef5f8858
[JFFS2 DBG] (2176) jffs2_truncate_fragtree: truncating fragtree to 0x00000696 bytes
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: read 40 bytes at 0x290aa0(0).
[JFFS2 DBG] (2019) read_more: read more 28 bytes
[JFFS2 DBG] (2019) jffs2_add_tn_to_tree: insert fragment 0x00-0x1f3, ver 1 at 00290aa0
[JFFS2 DBG] (2019) jffs2_lookup_tn: root c733dce8, offset 0
[JFFS2 DBG] (2019) jffs2_get_inode_nodes: nodes of inode #223 were read, the highest version is 1, latest_mctime 0, mctime_ver 0.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: tn ef31f8e8 ver 1 range 0x0-0x1f3 ov 0
[JFFS2 DBG] (2019) ver_insert: Link new node at c733dd04 (root is c733dd04)
[JFFS2 DBG] (2019) check_tn_node: check node 0x00-0x1f3, phys offs 0x290aa0
[JFFS2 DBG] (2019) check_node_data: check node at 0x290aa0, data length 144, partial CRC 0x000000, correct CRC 0xa444ebfd, data starts at 0x290.
[JFFS2 DBG] (2019) jffs2_build_inode_fragtree: Add ef31f8e8 (v 1, 0x0-0x1f3, ov 0) to fragtree
[JFFS2 DBG] (2019) jffs2_add_full_dnode_to_inode: adding node 0x00-0x1f3 @0x00290aa0 on flash, newfrag *c747b918
[JFFS2 DBG] (2019) jffs2_truncate_fragtree: truncating fragtree to 0x000001f3 bytes
[JFFS2 DBG] (2176) jffs2_do_read_inode: read inode #223
[JFFS2 DBG] (2176) jffs2_do_read_inode: waiting for ino #223 in state 1
[JFFS2 DBG] (2019) jffs2_kill_fragtree: killing
[JFFS2 DBG] (2176) jffs2_do_read_inode_internal: ino #223 pino/nlink is 1
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: ino #223
[JFFS2 DBG] (2176) jffs2_get_inode_nodes: read 40 bytes at 0x290aa0(2).
[JFFS2 DBG] (2176) read_more: read more 28 bytes
[JFFS2 DBG] (2176) jffs2_add_tn_to_tree: insert fragment 0x00-0x1f3, ver 1 at 00290aa0
[JFFS2 DBG] (2176) jffs2_lookup_tn: root c7617c18, of

Regards

Naresh

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,838件の閲覧回数
Pavel
NXP Employee
NXP Employee

Do you use SDK 1.9 and NOR Flash Deployment for this SDK?

See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,838件の閲覧回数
nareshpuli
Contributor III

Hi Pavel chubakov,

i am using SDK 1.7,  previously  board worked fine with same images but now show this issue , what could be the problem ?

regards

naresh

have a great day!!

0 件の賞賛
返信