Multiple interfaces working simultaneously on P1020RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple interfaces working simultaneously on P1020RDB

Jump to solution
3,974 Views
ayazshahid
Contributor I

Hi,

I can use all the three eTSEC controllers on my P1020RDB individually but I cannot use them all at the same time. My application needs to have more than one ports enabled at a time.

Has anyone got multiple eTSEC controllers working simultaneously on this board?

Thanks!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,823 Views
suchit_lepcha
NXP Employee
NXP Employee

Multiple eTSEC controllers should work. May I know more details of the problem you are facing? When you said "..but I cannot use them all at the same time.", what does that mean?

View solution in original post

0 Kudos
Reply
2 Replies
3,824 Views
suchit_lepcha
NXP Employee
NXP Employee

Multiple eTSEC controllers should work. May I know more details of the problem you are facing? When you said "..but I cannot use them all at the same time.", what does that mean?

0 Kudos
Reply
3,822 Views
ayazshahid
Contributor I

Thanks for your interest.

It actually turned out to be a problem with my driver it was overriding the buffer descriptors in TBASE registers.

My use case is to run eTSEC2, eTSEC3 and one of the ports from eTSEC1 controller simultaneously. The bug in my driver was corrupting buffer descriptors for all of them that's why I wasn't able to get it going.

0 Kudos
Reply