Multiple interfaces working simultaneously on P1020RDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Multiple interfaces working simultaneously on P1020RDB

跳至解决方案
3,900 次查看
ayazshahid
Contributor I

Hi,

I can use all the three eTSEC controllers on my P1020RDB individually but I cannot use them all at the same time. My application needs to have more than one ports enabled at a time.

Has anyone got multiple eTSEC controllers working simultaneously on this board?

Thanks!

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,749 次查看
suchit_lepcha
NXP Employee
NXP Employee

Multiple eTSEC controllers should work. May I know more details of the problem you are facing? When you said "..but I cannot use them all at the same time.", what does that mean?

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,750 次查看
suchit_lepcha
NXP Employee
NXP Employee

Multiple eTSEC controllers should work. May I know more details of the problem you are facing? When you said "..but I cannot use them all at the same time.", what does that mean?

0 项奖励
回复
3,748 次查看
ayazshahid
Contributor I

Thanks for your interest.

It actually turned out to be a problem with my driver it was overriding the buffer descriptors in TBASE registers.

My use case is to run eTSEC2, eTSEC3 and one of the ports from eTSEC1 controller simultaneously. The bug in my driver was corrupting buffer descriptors for all of them that's why I wasn't able to get it going.

0 项奖励
回复