More questions about the P1010 / P1014 I2C controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

More questions about the P1010 / P1014 I2C controller

1,165件の閲覧回数
ljp93105
Contributor I

A few days ago I asked about sample code for I2C in the U-boot sources, and was pointed to it.

I still have problems, and would like some guidance. When I take the controller out of reset, I find that the bus is busy, and the condition does not clear up even after waiting. If I go ahead and try to start a slave selection anyway, arbitration fails (not surprising).

 

I am using the P1010-RDB reference design board for my software development.

After system reset, I find the registers contain (as expected):

I2C_ADR = 00

I2C_FDR = 00

I2C_CR  = 00

I2C_SR  = 0x81 = MCF + RXAK

I2C_DR  = 00

I2C_DFSRR = 0x10

 

In my initialization routine, I set

I2C_FDR = 0x15 (with CCB clock at 400 MHz, that should yield an I2C clock at just under 2 kHz)

I2C_CR = 0x80

 

I now find that

I2C_SR = 0xA1 = MCF + MBB + RXAK

 

Where did the MBB (Bus Busy) come from ? How do I clear it ?

Am I supposed to set MSTA then clear it at initialization time ?

 

Message was edited by: Lars Poulsen I have attached the source code of my failing driver.

 

After initialization I get:

 

I2C Port 0 Interface Status

Registers: Adr=00

           FDR=07 factor=1024 freq=195312

           CR =80  MEN

           SR =B3  MCF MBB MAL MIF RXAK

           DR =00

           DFSRR=10

Data: State=00 RESET

 

I2C Port 1 Interface Status

Registers: Adr=00

           FDR=07 factor=1024 freq=195312

           CR =80  MEN

           SR =86  MCF SRW MIF

           DR =FF

         DFSRR=10

Data: State=00 RESET

 

Anyone have ideas ?

Original Attachment has been moved to: p10_i2c.c.zip

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

829件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached file. It is simple I2C example for the MPC8349. The P1010 I2C is similar to the MPC8349 I2C. Compare your code and this simple program example.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信