Model selector in P3041 ibis model

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Model selector in P3041 ibis model

ソリューションへジャンプ
2,346件の閲覧回数
petervuylsteke
Contributor I

Hi. In the ibis model of the P3041, a model selector 'bvdd_io' is used on e.g. the local bus signals. With the 'bvdd_io' model selector you can select 1 of 4 models going from  "3.3V I/O slowest slew rate" to " 3.3V I/O fastest slew rate"  All four models than have their 'minimum' 'typical' and 'maximum' simulation cases according the ibis specification.  As I don't see any setting to change drive strengths on the local bus, what is the relation between the slew rate model selector and the corner cases min-typ-max of the ibis file.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,951件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Sorry for delayed response

The output buffer has several options by design, but not all these options are available for user.

The only one option is available (permanently selected)

Please use option "01" - slow slew rate


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,952件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Sorry for delayed response

The output buffer has several options by design, but not all these options are available for user.

The only one option is available (permanently selected)

Please use option "01" - slow slew rate


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,951件の閲覧回数
petervuylsteke
Contributor I

Thanks for your answer. 

Is this valid for all models in the ibis file which have the model selector based on slew rate ?

Peter

0 件の賞賛
返信