Machine check error with LD with LDG set

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Machine check error with LD with LDG set

1,308件の閲覧回数
richardvandebun
Contributor I

On a p2041 a machine check exception is raised with LD and LDG bits sets. From the datasheet the errors could be cache parity errors, which to me are CPU silicon faults, or L2MMU multi-way hit or CoreNet Bad Data. 

I want to know what can cause the latter two errors. Can someone please explain the two errors?LDandLDGError.PNG

0 件の賞賛
返信
1 返信

1,225件の閲覧回数
ufedor
NXP Employee
NXP Employee

For the "L2MMU multi-way hit" description please refer to the e500mc Core Reference Manual, Table 4-5. Machine Check Exception Sources.

The "CoreNet Bad Data" condition is described after the Table 4-6. Error Report Definitions of the e500mc Core Reference Manual.

0 件の賞賛
返信