MMU TLB Initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMU TLB Initialization

Jump to solution
2,694 Views
frankdischner
Contributor I

Hello,

Is there any documentation about the 128-bit values used to initialize the TLB entries within the tcl scripts? I mean the lines that look like this:

# define   1GB TLB entry  7: 0x00000000 - 0x3FFFFFFF for DDR cacheable

    reg ${CAM_GROUP}L2MMU_CAM7 = 0xA00000061C0800000000000000000001

   

I haven't found anything in the reference manuals that match these values, but it's possible that I'm not looking in the right place.

This is what I've been able to deduce so far, but I'm not sure it's correct:

First word: Some size value in the upper bits, WIMGE in the lower bits

Second word: No idea, seems to always be 1C080000

Third word: Start address

Fourth word: Same as third word, but with lowest bit set (no idea what that bit signifies)

What I'm most interested in are the WIMGE bits. Judging by the values and comments in the default scripts, it seems that these are mapped directly to the lowest bits in the first word. So in the example above, the value of 6 means that the M and G bits are set and a value of E would mean bits I, M and G are set. Is that correct? If so, is there a reason that the DRAM is marked as guarded by default?

Thanks,

-Frank

Labels (1)
0 Kudos
Reply
1 Solution
2,353 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please take a look at chapter 5.10.5.4 TLB Register Details from Targeting_PA_Processors.pdf manual (PA\Help\PDF). Here you'll find full details about these friendly registers.

By the way, we're using this friendly format to avoid the users struggling with the initialization of the MAS0-4 registers.


Regards,

Marius

View solution in original post

0 Kudos
Reply
2 Replies
2,354 Views
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please take a look at chapter 5.10.5.4 TLB Register Details from Targeting_PA_Processors.pdf manual (PA\Help\PDF). Here you'll find full details about these friendly registers.

By the way, we're using this friendly format to avoid the users struggling with the initialization of the MAS0-4 registers.


Regards,

Marius

0 Kudos
Reply
2,353 Views
frankdischner
Contributor I

Thanks Marius, this is exactly what I was looking for.

-Frank

0 Kudos
Reply