Linux p5020 error message: Qman ErrInt: Corenet Initiator Data Error?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux p5020 error message: Qman ErrInt: Corenet Initiator Data Error?

2,499 次查看
chrisbrewer
Contributor I

I have a customer using the p5020 with Linux and at boot-time he's receiving the following error message:

     Qman ErrInt: Corenet Initiator Data Error

Can anyone provide some background as to what this means and what might be causing it?

Thanks in advance,

Chris B.

标签 (1)
标记 (4)
0 项奖励
回复
3 回复数

2,115 次查看
sedat_altun
Contributor III

Hi Sir,

I have also the same problem with P4080DS. Did you resolve the problem?

0 项奖励
回复

2,115 次查看
lunminliang
NXP Employee
NXP Employee

Haven't seem this kind of error on p5020 board with default settings.

Please clarify what board jumper settings and kernel configurations you're using so that reproduce it.


0 项奖励
回复

2,115 次查看
lunminliang
NXP Employee
NXP Employee

The error message indicates that bit 2 of "QMan error interrupt status register" asserted (CIDE). This interrupt is asserted if a beat of read with an error indication asserted is received by QMan as an initiator. Transactions initiated by either the QMan or BMan cause this bit to assert. Because QMan provides the initiator interface for both the QMan and BMan, the QMan reports this error on behalf of both, and the BMan does not report this error.

0 项奖励
回复