Linux booting problem in P4080 based system.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux booting problem in P4080 based system.

1,895件の閲覧回数
amitshah1
Contributor II

Hi All,

I'm working on P4080 based system with Linux running on it.

I'm facing an issue @ linux boot-up. Please share me your ideas regarding this.

It comes as:

===================================================================================

Machine check in kernel mode.

Caused by (from MCSR=8000): Load Error Report

Oops: Machine check, sig: 7 [#1]

SMP NR_CPUS=8 CoreNet Generic

Modules linked in:

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a #23

task: ee084a30 ti: efbae000 task.ti: ee0a2000

NIP: c01ef070 LR: c01ef060 CTR: 00000000

REGS: efbaff10 TRAP: 0204   Not tainted  (3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a)

MSR: 00029002 <CE,EE,ME>  CR: 84844e48  XER: 00000000

GPR00: c01ef01c ee0a3c30 ee084a30 f1049040 c0325214 c03b9ec4 ee1d2ba0 00000fe4

GPR08: 38241215 00000000 f104a278 38241215 84844e88 00000000 c00027f0 00000000

GPR16: 00000000 20000000 00000000 c039222c 00500001 ed010d20 00000002 c02a230c

GPR24: c03b1044 c02a21f0 c0389fb8 ee2810c0 00000000 ee1d6400 00000000 f1048000

NIP [c01ef070] n_tty_open+0x70/0x130

LR [c01ef060] n_tty_open+0x60/0x130

Call Trace:

[ee0a3c30] [c01ef01c] n_tty_open+0x1c/0x130 (unreliable)

[ee0a3c50] [c01f3c1c] tty_ldisc_open.isra.6+0x5c/0xa0

[ee0a3c60] [c01f4544] tty_ldisc_setup+0x24/0xc0

[ee0a3c80] [c01eb698] tty_init_dev+0xb8/0x1e0

[ee0a3ca0] [c01ec3b0] tty_open+0x330/0x680

[ee0a3d00] [c00eaedc] chrdev_open+0xbc/0x1c0

[ee0a3d30] [c00e3dc0] do_dentry_open.isra.15+0x190/0x2b0

[ee0a3d50] [c00e3f0c] finish_open+0x2c/0x60

[ee0a3d60] [c00f504c] do_last.isra.47+0x3fc/0xbe0

[ee0a3dd0] [c00f58e4] path_openat+0xb4/0x640

[ee0a3e30] [c00f6cb0] do_filp_open+0x30/0x90

[ee0a3eb0] [c00e52f8] do_sys_open+0x148/0x280

[ee0a3ef0] [c03558fc] kernel_init_freeable+0x160/0x1d0

[ee0a3f20] [c0002808] kernel_init+0x18/0x170

[ee0a3f40] [c000fca4] ret_from_kernel_thread+0x5c/0x64

Instruction dump:

913f0034 388451f8 4be8e5a9 3c80c032 387f2270 7fc5f378 38845214 4be8e595

93fd01a0 3bc00000 93df2244 387f1040 <893f003d> 38800000 93df0004 38a00200

---[ end trace 91dd2f21b34be299 ]---

Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000007

Rebooting in 180 seconds.

===================================================================================

Regards,

Amit Shah

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,448件の閲覧回数
amitshah1
Contributor II

Hi,

Above kernel booting problem solved when i passed only 2GB ddr3 size in u-boot bootargs which actually has 4GB ddr3 memory. I've enabled 4GB(2GB per ddr3 controller) in u-boot with using 36-bit physical addressing.

Also in u-boot bootup , it says 2GB left unmapped, which later on came to know that P4080 platform specific ddr initialization is using max 2GB size.

But, the problem is when i don't specify 2GB bootargs memory size,here kernel is crashing giving above error message.

I've enabled "large physical address support" and SWIOTLB options in kernel also, still giving same error. Device tree file also using 36-bit physical addressing.

Is there anything still we have to enable to use 4GB memory in Linux? Please share your ideas guys..

Amit Shah