Linux boot hang on P1020RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux boot hang on P1020RDB

2,862件の閲覧回数
fahadarslan
Contributor II

Hi,

I'm working on P1020RDB and using FSL SDK version 1.4. I've modified machine conf file so that p1020rdb.dts is used instead of p1020rdb-pd_32b.dts as below.

KERNEL_DEVICETREE = "${S}/arch/powerpc/boot/dts/p1020rdb.dts"

Now when I try to boot images generated with above change, boot process hangs at Freescale On-Chip EHCI Host Controller as can be seen in below log.

..

..

..

fsl-gianfar ethernet.3 eth2: TX BD ring size for Q[7]: 256

ucc_geth: QE UCC Gigabit Ethernet Controller

e1000e: Intel(R) PRO/1000 Network Driver - 2.1.4-k

e1000e: Copyright(c) 1999 - 2012 Intel Corporation.

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-pci: EHCI PCI platform driver

ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 28, io mem 0xffe22000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

If I rebuild kernel with EHCI disabled, control reaches login prompt.

Any suggestion how can this be resolved?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,896件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please try whether could use p1020rdb-pc_32b.dts to boot your system up.

USB2 is shared with localbus, so it must be disabled by default. Here since U-Boot doesn't clear the status property when it enables USB2. OTOH, U-Boot does create a new node when there isn't any. So, just comment it out in the dts file.

0 件の賞賛
返信

1,896件の閲覧回数
fahadarslan
Contributor II

I've tried using p1020rdb-pc_32b.dts, please see the log below:

fsl-gianfar ethernet.3 eth2: TX BD ring size for Q[7]: 256

ucc_geth: QE UCC Gigabit Ethernet Controller

e1000e: Intel(R) PRO/1000 Network Driver - 2.1.4-k

e1000e: Copyright(c) 1999 - 2012 Intel Corporation.

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-pci: EHCI PCI platform driver

ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver

/soc@ffe00000/usb@22000: Invalid 'dr_mode' property, fallback to host mode

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 28, io mem 0xffe22000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

/soc@ffe00000/usb@23000: Invalid 'dr_mode' property, fallback to host mode

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

0 件の賞賛
返信

1,896件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I think this kernel log is for p1020rdb.dts, because in p1020rdb-pc.dtsi, there is no property dr_mode, and node "usb@23000" is commented.

Previously I didn't ask which target board you used, if you use P1020rdb-PA or P1020rdb-PB, please choose the dtb file p1020rdb.dts, if you use P1020RDB-PC, please choose p1020rdb-pc_32b.dts.

For your problem, on P1020RDB board, USB2 is shared with local bus, so you need to comment the node "usb@23000" in dtb file, when boot from NOR Flash.

Please check the p1020rdb-pc.dtsi file in the Kernel source build_<target>_release/tmp/work/<target>-fsl_networking-linux/linux-qoriq-sdk/3.8-r11.1/git/arch/powerpc/boot/dts.

You could get Kernel source with the command

->bitbake virtual/kernel -c patch -f

After modify KERNEL_DEVICETREE variable, please make sure that Kernel is rebuilt.

->bitbake virtual/kernel -c compile -f

->bitbake virtual/kernel

0 件の賞賛
返信