JTAG Connection,failed to reset the target.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG Connection,failed to reset the target.

1,213件の閲覧回数
ruihuang
Contributor I

Hi,our core board are designed based on the P1020 processor,which has two DDR3 and one NOR flash. The JTAG interface has connected to the P1020 directly ,including SRESET,HRESET and TRST. But the DDR3 and NOR FLASH chips have no Power reset circuit or Reset chip.In this case,do the DDR3 and NOR FLASH reset signals have an effect on the core board Global reset? And does this unfavorable effect lead to the unsuccessful JTAG connection?

ラベル(1)
0 件の賞賛
返信
1 返信

963件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

I do not think missing power on reset circuit on NOR flash or DDR3 chips can corrupt debugger connection to the processor core.

Please check connections around the processor - reset configuration pins, clocking, reset circuit and etc.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信