IOMMU disable in kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IOMMU disable in kernel

3,554件の閲覧回数
emintz
Contributor I

Hi,

We have P2041RDB with DDC 1553 (Muxbus) PCIe card inside. In order to enable DMA mode of the card, the vendor requests to disable IOMMU support in the Linux kernel. The question is, what the impact of the IOMMU disabling? 

Thanks

0 件の賞賛
返信
1 返信

3,278件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Eli Mintz ,

 

PAMU(IOMMU) is used for hypervisor case. Typically, a PAMU resides astride the boundary between the coherency and I/O domains.

The FSL DPAA QBMAN drivers have an explicit dependency (for stashing) on the PAMU driver.

If you disable PAMU, then there would be issues with QBMAN drivers.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信