HugeTLBFS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HugeTLBFS

3,630 次查看
genuap
NXP Employee
NXP Employee

I'm considering using HugeTLBFS - I'm just wondering if anyone has implemented it before, and what your experience was.

And, as an additional question - has anyone ported it and used it under 32-bit linux?

Thanks,

Paul

标记 (2)
0 项奖励
回复
3 回复数

3,398 次查看
scottwood
NXP Employee
NXP Employee

HugeTLB is supported on recent 32-bit mpc85xx/QorIQ kernels, as long as you have large physical address support enabled.

0 项奖励
回复

3,398 次查看
genuap
NXP Employee
NXP Employee

Thanks - what about without large phys address (i.e. only 32-bit addressing). My understanding is that the MMU code is different and unsupported. Anyone ever try it or back-port it to a strictly 32-bit machine?

Thanks,

Paul

0 项奖励
回复

3,398 次查看
scottwood
NXP Employee
NXP Employee

It is not supported if large physical address support is turned off.  There should be no problem enabling large physical address support on any mpc85xx/QorIQ chip, even if the chip doesn't support 36-bit physical.  It's about Linux's internal data structures, not the hardware.

0 项奖励
回复