Have a great day,
The P1020 has COP/JTAG interface for external debugger and can boot under debugger control while there is not any other boot device. For exampe CodeWarrior can initialize the P1020 memory, download software and start it. The P1020 SD/MMC controller is compatible with MultiMediaCard System Specification, Version 4.2. It was issued when eMMC had not introduced yet. It can boot from the MMC card or from eMMC device while treat it as MMC card.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------