How to assign 4GB memory addresses to DDR in uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to assign 4GB memory addresses to DDR in uboot

2,356 Views
敏赵
Contributor I

Hi,

We have designed a product using p2020 cpu referring to the design of p2020rdb-pc board.

We changed the chip of DDR to 4GB.

My ddr is 2 rank, I have modify the following codes in p1_p2_rdb_pc.h:

#define CONFIG_SYS_SDRAM_SIZE_LAWLAW_SIZE_4G
#define CONFIG_CHIP_SELECTS_PER_CTRL 2

But I don't understand the following cods in board/freescale/p1_p2_rdb_pc/ tlb.c:

#if defined(CONFIG_SYS_RAMBOOT) || defined(CONFIG_SPL)

#ifdef CONFIG_SYS_INIT_L2_ADDR

  /* L2SRAM */

  SET_TLB_ENTRY(1, CONFIG_SYS_INIT_L2_ADDR, CONFIG_SYS_INIT_L2_ADDR_PHYS,

       MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

       0, 8, BOOKE_PAGESZ_256K, 1),

  SET_TLB_ENTRY(1, CONFIG_SYS_INIT_L2_ADDR + 0x40000,

       CONFIG_SYS_INIT_L2_ADDR_PHYS + 0x40000,

       MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

       0, 12, BOOKE_PAGESZ_256K, 1),

#else

  /* *I*G - eSDHC/eSPI/NAND boot */

  SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE, CONFIG_SYS_DDR_SDRAM_BASE,

  MAS3_SX|MAS3_SW|MAS3_SR, 0,

  0, 8, BOOKE_PAGESZ_1G, 1),

#if defined(CONFIG_P1020MBG) || defined(CONFIG_P1020RDB_PD)

  /* 2G DDR on P1020MBG, map the second 1G */

  SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE + 0x40000000,

  CONFIG_SYS_DDR_SDRAM_BASE + 0x40000000,

  MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

  0, 9, BOOKE_PAGESZ_1G, 1),

#endif /* P1020MBG */

#endif /* not L2 SRAM */

#endif /* RAMBOOT/SPL */

I found config_sys_init_l2_addr has been defined in p1_p2_rdb_pc.h. So did that mean there don't set tlb_entry 8 for ddr to p2020rdb-pc?

If I want to assign 4GB memory map to DDR, how should I modify the above codes in tlb.c?

Best regards,

Min Zhao

Labels (1)
0 Kudos
Reply
2 Replies

1,395 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Min Zhao,

Please refer the following source code from SDK 1.6, and please attach p1_p2_rdb_pc.h and tlb.c which you are using.

In addition, as we discussed previously, in u-boot, it is impossible to map the whole 4G DDR memory in MMU configuration, because u-boot is 32bit address space program(totally 4G).

Again, please learn the application note http://cache.freescale.com/files/32bit/doc/app_note/AN4064.pdf?&Parent_nodeId=&Parent_pageType=, especially the section "Utilizing 36-Bit Physical Addressing in U-Boot".

#if defined(CONFIG_SYS_RAMBOOT) || \

        (defined(CONFIG_SPL) && !defined(CONFIG_SPL_COMMON_INIT_DDR))

        /* *I*G - eSDHC/eSPI/NAND boot */

        SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE, CONFIG_SYS_DDR_SDRAM_BASE,

                        MAS3_SX|MAS3_SW|MAS3_SR, 0,

                        0, 8, BOOKE_PAGESZ_1G, 1),

#if defined(CONFIG_P1020MBG) || defined(CONFIG_P1020RDB_PD)

        /* 2G DDR on P1020MBG, map the second 1G */

        SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE + 0x40000000,

                        CONFIG_SYS_DDR_SDRAM_BASE + 0x40000000,

                        MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

                        0, 9, BOOKE_PAGESZ_1G, 1),

#endif /* P1020MBG */

#endif /* RAMBOOT/SPL */

#ifdef CONFIG_SYS_INIT_L2_ADDR

        /* *I*G - L2SRAM */

        SET_TLB_ENTRY(1, CONFIG_SYS_INIT_L2_ADDR, CONFIG_SYS_INIT_L2_ADDR_PHYS,

                      MAS3_SX|MAS3_SW|MAS3_SR, MAS2_G,

                      0, 11, BOOKE_PAGESZ_256K, 1),

#if CONFIG_SYS_L2_SIZE >= (256 << 10)

        SET_TLB_ENTRY(1, CONFIG_SYS_INIT_L2_ADDR + 0x40000,

                      CONFIG_SYS_INIT_L2_ADDR_PHYS + 0x40000,

                      MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

                      0, 12, BOOKE_PAGESZ_256K, 1)

#endif

#endif

Thanks,

Yiping

0 Kudos
Reply

1,395 Views
lunminliang
NXP Employee
NXP Employee

I think no if CONFIG_SYS_INIT_L2_ADDR defined.

Anyone could confirm?

0 Kudos
Reply