Help for a beginner with a TWR-P1025

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help for a beginner with a TWR-P1025

ソリューションへジャンプ
3,525件の閲覧回数
zenomaspoli
Contributor III

Hi everybody,

I'm a student and I recived from my professor a TWR-P1025

My assignment is to start using this module, and do some easy "hello world" exercise (led on/led of,....).

I've installed the Special Edition CW for Microcontrollers 10.5, but I'm not sure anymore

that is the one that I need. When I start a new MCU project I can not chose the device that I'm using,

the QorIQ family does not appear (during the insallation i've crossed all the family).
So i've been looking for something and I've found the "Processor Expert Software: QorIQ Configuration Suite".

It actually thise one that i need ? If yes, who I have to ask to? 'cause it's free, but they want me to give a name for the download.

Thank you guys ! 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,361件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee
0 件の賞賛
返信
7 返答(返信)
3,361件の閲覧回数
zenomaspoli
Contributor III

Hi,

I couldn't work for a while, but now i've downloaded the PA version.

I dont have a USBTAP, can I still download from CW on my twr through

the mini USB UART ?

0 件の賞賛
返信
3,361件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi,

Unfortunately, 1025-twr didn't come with a jtag probe integrated on board, so is necessary to have a USBTAP for download/debug.

Adrian

0 件の賞賛
返信
3,361件の閲覧回数
zenomaspoli
Contributor III

And wont the TWR-IND-IO be able to replace the USBTAP?

0 件の賞賛
返信
3,361件の閲覧回数
addiyi
NXP Employee
NXP Employee

I take a look on TWR-IND-IO and this module doesn't provide embedded usbtap, so will cannot replace the USBTAP.

Adrian

0 件の賞賛
返信
3,361件の閲覧回数
zenomaspoli
Contributor III

OK, thank you so much Adrian, really

0 件の賞賛
返信
3,362件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please use CW for PA (Power Architecture) 10.3 from here [1]

Regards,

Marius

[1] CodeWarrior Development Studio v10 for Power Architecture® Technology (Eclipse) Product Summary Page

0 件の賞賛
返信
3,361件の閲覧回数
zenomaspoli
Contributor III

Thanks Marius !

Actually that one was the first one that I've installed, but then I moved

to the Special Edition because of the trial.

Not a problem, ill go back on PA version.

I hope in 30 days my school have asked for an academic license.

Thanks again Marius! I feel I'll be back soon with new questions

0 件の賞賛
返信