Help for a beginner with a TWR-P1025

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Help for a beginner with a TWR-P1025

跳至解决方案
3,531 次查看
zenomaspoli
Contributor III

Hi everybody,

I'm a student and I recived from my professor a TWR-P1025

My assignment is to start using this module, and do some easy "hello world" exercise (led on/led of,....).

I've installed the Special Edition CW for Microcontrollers 10.5, but I'm not sure anymore

that is the one that I need. When I start a new MCU project I can not chose the device that I'm using,

the QorIQ family does not appear (during the insallation i've crossed all the family).
So i've been looking for something and I've found the "Processor Expert Software: QorIQ Configuration Suite".

It actually thise one that i need ? If yes, who I have to ask to? 'cause it's free, but they want me to give a name for the download.

Thank you guys ! 

标签 (1)
0 项奖励
回复
1 解答
3,367 次查看
marius_grigoras
NXP Employee
NXP Employee
0 项奖励
回复
7 回复数
3,367 次查看
zenomaspoli
Contributor III

Hi,

I couldn't work for a while, but now i've downloaded the PA version.

I dont have a USBTAP, can I still download from CW on my twr through

the mini USB UART ?

0 项奖励
回复
3,367 次查看
addiyi
NXP Employee
NXP Employee

Hi,

Unfortunately, 1025-twr didn't come with a jtag probe integrated on board, so is necessary to have a USBTAP for download/debug.

Adrian

0 项奖励
回复
3,367 次查看
zenomaspoli
Contributor III

And wont the TWR-IND-IO be able to replace the USBTAP?

0 项奖励
回复
3,367 次查看
addiyi
NXP Employee
NXP Employee

I take a look on TWR-IND-IO and this module doesn't provide embedded usbtap, so will cannot replace the USBTAP.

Adrian

0 项奖励
回复
3,367 次查看
zenomaspoli
Contributor III

OK, thank you so much Adrian, really

0 项奖励
回复
3,368 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please use CW for PA (Power Architecture) 10.3 from here [1]

Regards,

Marius

[1] CodeWarrior Development Studio v10 for Power Architecture® Technology (Eclipse) Product Summary Page

0 项奖励
回复
3,367 次查看
zenomaspoli
Contributor III

Thanks Marius !

Actually that one was the first one that I've installed, but then I moved

to the Special Edition because of the trial.

Not a problem, ill go back on PA version.

I hope in 30 days my school have asked for an academic license.

Thanks again Marius! I feel I'll be back soon with new questions

0 项奖励
回复