Hardware Simulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardware Simulator

2,799件の閲覧回数
jm1015
Contributor II

Is it possible to simulate and test the code for testing peripherals without hardware? My intended processor is P1015/1024 QorIQ processor. I am using GHS multi V7 . Is there any software plug in which help users in develop application before they get actual hardware?

ラベル(1)
3 返答(返信)

2,505件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Unfortunately, we do not offer software emulators to emulate P1015/1024 peripherals without hardware.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,505件の閲覧回数
jm1015
Contributor II

Thank you, Alexander.

Is it also not possible to simulate and verify eTSEC module also?

* via loop back

Regards,

J Mathew

0 件の賞賛
返信

2,505件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Unfortunately, we do not offer software emulator to emulate P1015/1024 eTSEC without hardware.