Generating SD Card Image for P2020 / T1042

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generating SD Card Image for P2020 / T1042

Jump to solution
2,443 Views
raratex
Contributor II

Hello community,

I am dealing with a problem with generating boot-image for following PowerPC/QorIQ Platforms:

- P2020
- T1042

My question is, can anybody give me some helpful info or links to information, how to generate an image for booting from SD card?
Especially, how to format sd card, where should be RCW placed, where PBL, U-Boot, DTB, and Linux ...?
Are there any tools or scripts under Linux/Yocto ..?

Thanks for the help!

Regards
Radek

Labels (2)
0 Kudos
Reply
1 Solution
2,093 Views
ufedor
NXP Employee
NXP Employee

For the P2020 please refer to the NXP Linux SDK v1.9 Knowledge Center, 10.1 eSPI/SD/NAND Boot and 4.4.8.6.4 SD Deployment available at:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427 

For the T1042 the NXP Linux SDK v2.0 is capable to generate complete SD card image (u-boot-sdcard) which has to be written to the SD card from offset block 8. For the deployment refer to the NXP Linux SDK v2.0 Documentation:

Submit Form 

View solution in original post

1 Reply
2,094 Views
ufedor
NXP Employee
NXP Employee

For the P2020 please refer to the NXP Linux SDK v1.9 Knowledge Center, 10.1 eSPI/SD/NAND Boot and 4.4.8.6.4 SD Deployment available at:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427 

For the T1042 the NXP Linux SDK v2.0 is capable to generate complete SD card image (u-boot-sdcard) which has to be written to the SD card from offset block 8. For the deployment refer to the NXP Linux SDK v2.0 Documentation:

Submit Form