Dear all,
I have loaded the compiled QorIQ-SDK-V1.2-20120614-yocto linux kernel module on p1021 (2C, 900M) based board and get into linux prompt. Then I try to let it support for i2c interface.
I have modified menuconfig like below:
<*> I2C/SMBus Test StubAnd modified device tree as below:
soc@ffe00000 {
ranges = <0x0 0x0 0xffe00000 0x100000>;
#address-cells = <0x1>;
#size-cells = <0x1>;
device_type = "soc";
compatible = "fsl,p1021-immr", "simple-bus";
bus-frequency = <0x0>;
i2c1: i2c@3000 {
status = "okay";
#address-cells = <0x1>;
#size-cells = <0x0>;
cell-index = <0x0>;
compatible = "fsl-i2c";
reg = <0x3000 0x100>;
interrupts = <0x2b 0x2 0x0 0x0>;
dfsrr;
};
i2c2: i2c@3100 {
status = "okay";
#address-cells = <0x1>;
#size-cells = <0x0>;
cell-index = <0x1>;
compatible = "fsl-i2c";
reg = <0x3100 0x100>;
interrupts = <0x2b 0x2 0x0 0x0>;
dfsrr;
};
...
};After load the kernel, I can't see any i2c device in /dev/ directory (dev/i2c-0 and dev/i2c-1). And can't see any file in /sys/class/i2c-dev/ directory.
root@p1021rdb:/# ls /dev/i2c* ls: /dev/i2c*: No such file or directory root@p1021rdb: root@p1021rdb:~# ls /sys/class/i2c-dev/ root@p1021rdb:
And I try to modify menuconfig to set I2C device interface as modularizes (<M> I2C device interface). But when I use modprobe command, it show below error.
root@p1021rdb:/mnt# modprobe i2c-dev modprobe: module i2c-dev not found in modules.dep
Can someone guide me how to resolve this issue? What could be going wrong here?
Thanks for your help,
Best Regards,
Henry
Test interrupts on your board using the following command:
cat /proc/interrupts
Is there interrupt from I2C?
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------