Can anyone suggest RGMII layout guidelines for P2041?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can anyone suggest RGMII layout guidelines for P2041?

3,445件の閲覧回数
avinashh
Contributor III

Can anyone suggest RGMII layout guidelines for P2041?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,390件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

See for example 

http://www.icplus.com.tw/Data/Application%20Note/IP1001%20PCB%20layout%20guideline%20Apr%2017%20V15....

The P2041 RGMII implies that PC board design requires clocks to be routed such that an additional trace delay of greater than 1.5 ns is added to the associated clock signal. Many PHY vendors already incorporate the necessary delay inside their chip. If so, additional PCB delay is probably not needed.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信