Hi,I am developing the P1010's Linux system using YOCTO. The U-BOOT has finished, uImage and dtb have download into the nor flash in board. However, The linux system can not enter the login, and does't print anything, the LOG shows as follow:
U-Boot 2014.01QorIQ-SDK-V1.6+gfe1d4f5 (Sep 30 2016 - 12:23:11)
CPU: P1010, Version: 2.0, (0x80f10020)
Core: e500, Version: 5.2, (0x80212152)
Clock Configuration:
CPU0:800 MHz,
CCB:400 MHz,
DDR:400 MHz (800 MT/s data rate) (Asynchronous), IFC:100 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Board: P1010RDB-PB, Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
i2c_wait: No RXACK
CPLD: v0.0, Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
i2c_wait: No RXACK
i2c_wait: No RXACK
PCB: v1.0, Boot from: Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
i2c_wait: No RXACK
i2c_wait: No RXACK
NOR vBank1
I2C: Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
ready
SPI: ready
DRAM: Configuring DDR for 800 MT/s data rate
total 1 GB
Need to wait up to 66 * 10ms
dram_size_Pre = 40000000
setup_ddr_tlbs_phys OK
Have jump the setup_ddr_tlbs_phys!
dram_size = 40000000
DDR: gd->ram_size ok
1 GiB1 GiB (DDR3, 32-bit, CL=6, ECC off)
Jump the sequence!
Top of RAM usable for U-Boot at: 40000000
Reserving 2562k for U-Boot at: 3fd70000
Reserving 1032k for malloc() at: 3fc6e000
Reserving 72 Bytes for Board Info at: 3fc6dfb8
Reserving 164 Bytes for Global Data at: 3fc6df14
Stack Pointer at: 3fc6df00
New Stack Pointer is: 3fc6df00
Now running in RAM - U-Boot at: 3fd70000
set_tlb OK!
Flash: flash detect cfi
fwc addr fe000000 cmd f0 f0 8bit x 8 bit
fwc addr fe000000 cmd ff ff 8bit x 8 bit
fwc addr fe000055 cmd 98 98 8bit x 8 bit
is= cmd 51(Q) addr fe000010 is= ff 51
fwc addr fe000555 cmd 98 98 8bit x 8 bit
is= cmd 51(Q) addr fe000010 is= ff 51
fwc addr fe000000 cmd f0 f0f0 16bit x 8 bit
fwc addr fe000000 cmd ff ffff 16bit x 8 bit
fwc addr fe0000aa cmd 98 9898 16bit x 8 bit
is= cmd 51(Q) addr fe000020 is= 0051 5151
fwc addr fe000aaa cmd 98 9898 16bit x 8 bit
is= cmd 51(Q) addr fe000020 is= 0051 5151
fwc addr fe000000 cmd f0 00f0 16bit x 16 bit
fwc addr fe000000 cmd ff 00ff 16bit x 16 bit
fwc addr fe0000aa cmd 98 0098 16bit x 16 bit
is= cmd 51(Q) addr fe000020 is= 0051 0051
is= cmd 52(R) addr fe000022 is= 0052 0052
is= cmd 59(Y) addr fe000024 is= 0059 0059
device interface is 2
found port 2 chip 2 port 16 bits chip 16 bits
00 : 51 52 59 02 00 40 00 00 00 00 00 27 36 00 00 06 QRY..@.....'6...
10 : 06 09 13 03 05 03 02 1b 02 00 06 00 01 ff 03 00 ................
20 : 02 00 00 00 00 00 00 00 00 00 00 00 00 00 08 d1 ................
fwc addr fe000000 cmd f0 00f0 16bit x 16 bit
fwc addr fe000aaa cmd aa 00aa 16bit x 16 bit
fwc addr fe000554 cmd 55 0055 16bit x 16 bit
fwc addr fe000aaa cmd 90 0090 16bit x 16 bit
fwc addr fe000000 cmd f0 00f0 16bit x 16 bit
fwc addr fe0000aa cmd 98 0098 16bit x 16 bit
manufacturer is 2
manufacturer id is 0x1
device id is 0x227e
device id2 is 0x2801
cfi version is 0x3133
size_ratio 1 port 16 bits chip 16 bits
found 1 erase regions
erase region 0: 0x020003ff
erase_region_count = 1024 erase_region_size = 131072
ERROR: too many flash sectors
fwc addr fe000000 cmd f0 00f0 16bit x 16 bit
128 MiB
L2: 256 KiB enabled
PORDEVSR[IO_SEL_SRDS] = 2
NAND: 2048 MiB
MMC: FSL_SDHC: 0
*** Warning - bad CRC, using default environment
Destroy Hash Table: 3fe080ac table = 00000000
Create Hash Table: N=294
INSERT: table 3fe080ac, filled 1/307 rv 3fc716f8 ==> name="bootcmd" value="setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs; cp.b ff400000 2000000 300000;cp.b ff000000 10000000 400000;cp.b ff700000 c00000 4000;bootm 10000000 2000000 c00000"
INSERT: table 3fe080ac, filled 2/307 rv 3fc713ec ==> name="ramboot" value="setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs; cp.b ff400000 2000000 300000;cp.b ff000000 10000000 400000;cp.b ff700000 c00000 4000;bootm 10000000 2000000 c00000"
INSERT: table 3fe080ac, filled 3/307 rv 3fc72918 ==> name="bootdelay" value="10"
INSERT: table 3fe080ac, filled 4/307 rv 3fc72594 ==> name="baudrate" value="115200"
DELETE CANDIDATE: "loads_echo"
hdelete: DELETE key "loads_echo"
DELETE ERROR ##############################
INSERT: table 3fe080ac, filled 5/307 rv 3fc71ae0 ==> name="ethaddr" value="00:E0:0C:BC:E5:60"
INSERT: table 3fe080ac, filled 6/307 rv 3fc715a4 ==> name="ethprime" value="eTSEC1"
INSERT: table 3fe080ac, filled 7/307 rv 3fc71e3c ==> name="ipaddr" value="192.168.0.100"
INSERT: table 3fe080ac, filled 8/307 rv 3fc7139c ==> name="serverip" value="192.168.0.3"
INSERT: table 3fe080ac, filled 9/307 rv 3fc7279c ==> name="rootpath" value="/opt/nfsroot"
INSERT: table 3fe080ac, filled 10/307 rv 3fc71590 ==> name="gatewayip" value="192.168.0.1"
INSERT: table 3fe080ac, filled 11/307 rv 3fc718c4 ==> name="netmask" value="255.255.255.0"
INSERT: table 3fe080ac, filled 12/307 rv 3fc71450 ==> name="hostname" value="unknown"
INSERT: table 3fe080ac, filled 13/307 rv 3fc71e28 ==> name="bootfile" value="uImage"
INSERT: table 3fe080ac, filled 14/307 rv 3fc7161c ==> name="loadaddr" value="1000000"
INSERT: table 3fe080ac, filled 15/307 rv 3fc724cc ==> name="hwconfig" value="CONFIG_DEF_HWCONFIG"
INSERT: table 3fe080ac, filled 16/307 rv 3fc71dec ==> name="netdev" value="eth0"
INSERT: table 3fe080ac, filled 17/307 rv 3fc7210c ==> name="uboot" value="u-boot.bin"
INSERT: table 3fe080ac, filled 17/307 rv 3fc7161c ==> name="loadaddr" value="1000000"
INSERT: table 3fe080ac, filled 18/307 rv 3fc718b0 ==> name="consoledev" value="ttyS0"
INSERT: table 3fe080ac, filled 19/307 rv 3fc71b6c ==> name="ramdiskaddr" value="2000000"
INSERT: table 3fe080ac, filled 20/307 rv 3fc71a90 ==> name="ramdiskfile" value="rootfs.ext2.gz.uboot"
INSERT: table 3fe080ac, filled 21/307 rv 3fc71f18 ==> name="fdtaddr" value="c00000"
INSERT: table 3fe080ac, filled 22/307 rv 3fc71734 ==> name="fdtfile" value="p1010rdb.dtb"
INSERT: table 3fe080ac, filled 23/307 rv 3fc71310 ==> name="bdev" value="sda1"
INSERT: table 3fe080ac, filled 23/307 rv 3fc724cc ==> name="hwconfig" value="usb1:dr_mode=host,phy_type=utmi"
INSERT: table 3fe080ac, filled 24/307 rv 3fc71a04 ==> name="othbootargs" value="ramdisk_size=600000"
INSERT: table 3fe080ac, filled 25/307 rv 3fc717ac ==> name="usbfatboot" value="setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs; usb start;fatload usb 0:2 $loadaddr $bootfile;fatload usb 0:2 $fdtaddr $fdtfile;fatload usb 0:2 $ramdiskaddr $ramdiskfile;bootm $loadaddr $ramdiskaddr $fdtaddr"
INSERT: table 3fe080ac, filled 26/307 rv 3fc7242c ==> name="usbext2boot" value="setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs; usb start;ext2load usb 0:4 $loadaddr $bootfile;ext2load usb 0:4 $fdtaddr $fdtfile;ext2load usb 0:4 $ramdiskaddr $ramdiskfile;bootm $loadaddr $ramdiskaddr $fdtaddr"
INSERT: table 3fe080ac, filled 27/307 rv 3fc714dc ==> name="boot_bank0" value="i2c dev 0; i2c mw 18 1 fe; i2c mw 18 3 0;i2c mw 19 1 2; i2c mw 19 3 e1; reset"
INSERT: table 3fe080ac, filled 28/307 rv 3fc72ae4 ==> name="boot_bank1" value="i2c dev 0; i2c mw 18 1 fe; i2c mw 18 3 0;i2c mw 19 1 12; i2c mw 19 3 e1; reset"
INSERT: table 3fe080ac, filled 29/307 rv 3fc72544 ==> name="boot_nand" value="i2c dev 0; i2c mw 18 1 fc; i2c mw 18 3 0;i2c mw 19 1 8; i2c mw 19 3 f7; reset"
INSERT: table 3fe080ac, filled 30/307 rv 3fc71950 ==> name="boot_spi" value="i2c dev 0; i2c mw 18 1 fa; i2c mw 18 3 0;i2c mw 19 1 0; i2c mw 19 3 f7; reset"
INSERT: table 3fe080ac, filled 31/307 rv 3fc721d4 ==> name="boot_sd" value="i2c dev 0; i2c mw 18 1 f8; i2c mw 18 3 0;i2c mw 19 1 4; i2c mw 19 3 f3; reset"
INSERT: free(data = 3fc70bb8)
INSERT: done
EEPROM: Requested speed:400000, i2c_clk:200000000
FDR:0x28, div:640, ga:0x4, gb:0x2, a:10, b:64, speed:312500
Tr <= 170 ns
FDR:0x27, div:512, ga:0x7, gb:0x1, a:16, b:32, speed:390625
Tr <= 10 ns
divider:500, est_div:512, DFSR:10
FDR:0x27, speed:390625
i2c_wait: No RXACK
i2c_wait: No RXACK
ID: SN:
Errata:
Build date: 2000/00/00 00:00:00
CRC: 00000000 (should be 395d7a27)
EEPROM dump: (0x7c bytes)
00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
70: 00 00 00 00 00 00 00 00 00 00 00 00
Read failed.
In: serial
Out: serial
Err: serial
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
i2c_wait: No RXACK
U-Boot relocated to 3fd70000
Net: lcd initialzing!
wait lcd 1...
wait lcd 2...
wait lcd 3...
wait lcd 4...
wait lcd 5...
wait lcd 10...
*(unsigned short *)(&lcd_screen_image[0]) = 1f
wait lcd 11........
wait lcd 6....................
wait lcd 12............
wait lcd 10...
*(unsigned short *)(&lcd_screen_image[0]) = 1f
wait lcd 11........
BCM5396 initialzing!
TSECs initializing
Initial value for argc=3
Final value for argc=3
Phy not found
PHY reset timed out
eTSEC1 connected to Generic PHY
Phy not found
PHY reset timed out
eTSEC2 connected to Generic PHY
Phy not found
PHY reset timed out
eTSEC3 connected to Generic PHY
eTSEC1 [PRIME], eTSEC2, eTSEC3
### main_loop entered: bootdelay=10
### main_loop: bootcmd="setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs; cp.b ff400000 2000000 300000;cp.b ff000000 10000000 400000;cp.b ff700000 c00000 4000;bootm 10000000 2000000 c00000"
Hit any key to stop autoboot: 10 9 0
=> boot
Initial value for argc=6
Final value for argc=6
WARNING: adjusting available memory to 30000000
## Current stack ends at 0x3fc6db18
* kernel: cmdline image address = 0x10000000
## Booting kernel from Legacy Image at 10000000 ...
Image Name: Linux-3.12.19-rt30-QorIQ-SDK-V1.
Created: 2016-10-08 8:26:28 UTC
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 3920505 Bytes = 3.7 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
kernel data at 0x10000040, len = 0x003bd279 (3920505)
* ramdisk: cmdline image address = 0x02000000
## Loading init Ramdisk from Legacy Image at 02000000 ...
Image Name: fsl-image-minimal-p1010rdb-20160
Created: 2016-09-29 12:48:39 UTC
Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
Data Size: 2970697 Bytes = 2.8 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
ramdisk start = 0x02000040, ramdisk end = 0x022d5489
* fdt: cmdline image address = 0x00c00000
## Checking for 'FDT'/'FDT Image' at 00c00000
Wrong FIT format: no description
* fdt: raw FDT blob
## Flattened Device Tree blob at 00c00000
Booting using the fdt blob at 0xc00000
of_flat_tree at 0x00c00000 size 0x00002cfd
Initial value for argc=3
Final value for argc=3
Uncompressing Kernel Image ... OK
kernel loaded at 0x00000000, end = 0x0079f6a0
## cmdline at 0x03ffff00 ... 0x03ffff39
## initrd_high = 0xffffffff, copy_to_ram = 1
Loading Ramdisk to 2fd2a000, end 2ffff449 ... OK
ramdisk load start = 0x2fd2a000, ramdisk load end = 0x2ffff449
## device tree at 00c00000 ... 00c02cfc (len=23805 [0x5CFD])
Loading Device Tree to 03ffa000, end 03fffcfc ... OK
Initial value for argc=3
Final value for argc=3
No alias for ethernet0
Updating property 'bd-stash' =
Updating property 'rx-stash-len' = 00 00 00 60
Updating property 'rx-stash-idx' = 00 00 00 00
Updating property 'bd-stash' =
Updating property 'rx-stash-len' = 00 00 00 60
Updating property 'rx-stash-idx' = 00 00 00 00
Updating property 'timebase-frequency' = 02 fa f0 80
Updating property 'bus-frequency' = 17 d7 84 00
Updating property 'bus-frequency' = 17 d7 84 00
Updating property 'bus-frequency' = 05 f5 e1 00
Updating property 'bus-frequency' = 05 f5 e1 00
Updating property 'clock-frequency' = 17 d7 84 00
Updating property 'clock-frequency' = 17 d7 84 00
Updating property 'clock-frequency' = 17 d7 84 00
Updating property 'status' = 6f 6b 61 79 00
Updating property 'timer-frequency' = 0b eb c2 00
Updating property 'clock_freq' = 0b eb c2 00
Updating property 'clock-frequency' = 0b eb c2 00
Updating property 'clock-frequency' = 0b eb c2 00
OF: ** translation for device serial@4500 **
OF: bus is default (na=1, ns=1) on soc@d8000000
OF: translating address: 00004500
OF: parent bus is default (na=2, ns=2) on
OF: walking ranges...
OF: default map, cp=0, s=100000, da=4500
OF: parent translation for: 00000000 d8000000
OF: with offset: 4500
OF: one level translation: 00000000 d8004500
OF: reached root node
OF: ** translation for device serial@4600 **
OF: bus is default (na=1, ns=1) on soc@d8000000
OF: translating address: 00004600
OF: parent bus is default (na=2, ns=2) on
OF: walking ranges...
OF: default map, cp=0, s=100000, da=4600
OF: parent translation for: 00000000 d8000000
OF: with offset: 4600
OF: one level translation: 00000000 d8004600
OF: reached root node
No alias for ethernet0
OF: ** translation for device soc@d8000000 **
OF: bus is default (na=2, ns=2) on
OF: translating address: 00000000 d8000000
OF: reached root node
OF: ** translation for device serial@4500 **
OF: bus is default (na=1, ns=1) on soc@d8000000
OF: translating address: 00004500
OF: parent bus is default (na=2, ns=2) on
OF: walking ranges...
OF: default map, cp=0, s=100000, da=4500
OF: parent translation for: 00000000 d8000000
OF: with offset: 4500
OF: one level translation: 00000000 d8004500
OF: reached root node
OF: ** translation for device serial@4600 **
OF: bus is default (na=1, ns=1) on soc@d8000000
OF: translating address: 00004600
OF: parent bus is default (na=2, ns=2) on
OF: walking ranges...
OF: default map, cp=0, s=100000, da=4600
OF: parent translation for: 00000000 d8000000
OF: with offset: 4600
OF: one level translation: 00000000 d8004600
OF: reached root node
## Transferring control to Linux (at address 00000000) ...
Booting using OF flat tree...
Using P1010 RDB machine description
Memory CAM mapping: 256/256/256 Mb, residual: 256Mb
Linux version 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a (freescale@freescale-sdk) (gcc version 4.8.1 (GCC) ) #2 Sat Oct 8 16:25:35 CST 2016
Found initrd at 0xefd2a000:0xeffff449
bootconsole [udbg0] enabled
setup_arch: bootmem
p1010_rdb_setup_arch()
P1010 RDB board from Freescale Semiconductor
arch: exit
Zone ranges:
DMA [mem 0x00000000-0x2fffffff]
Normal empty
HighMem [mem 0x30000000-0x3fffffff]
Movable zone start for each node
Early memory node ranges
node 0: [mem 0x00000000-0x3fffffff]
MMU: Allocated 1088 bytes of context maps for 255 contexts
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260608
Kernel command line: root=/dev/ram rw console=ttyS0,115200 ramdisk_size=600000
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Sorting __ex_table...
Memory: 961592K/1048576K available (5628K kernel code, 268K rwdata, 1668K rodata, 228K init, 1201K bss, 86984K reserved, 262144K highmem)
Kernel virtual memory layout:
* 0xfffcf000..0xfffff000 : fixmap
* 0xffc00000..0xffe00000 : highmem PTEs
* 0xffbfe000..0xffc00000 : early ioremap
* 0xf1000000..0xffbfe000 : vmalloc & ioremap
SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at d8040000, max 1 CPUs
mpic: ISU size: 256, shift: 8, mask: ff
mpic: Initializing for 256 sources
clocksource: timebase mult[14000000] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
devtmpfs: initialized
NET: Registered protocol family 16
PCI: Probing PCI hardware
fsl-l2ctlr d8020000.l2-cache-controller: Entire L2 as cache, provide valid sram address and size
fsl-l2ctlr: probe of d8020000.l2-cache-controller failed with error -22
bio: create slab <bio-0> at 0
Freescale Elo series DMA driver
fsl-elo-dma d8021300.dma: #0 (fsl,eloplus-dma-channel), irq 20
fsl-elo-dma d8021300.dma: #1 (fsl,eloplus-dma-channel), irq 21
fsl-elo-dma d8021300.dma: #2 (fsl,eloplus-dma-channel), irq 22
fsl-elo-dma d8021300.dma: #3 (fsl,eloplus-dma-channel), irq 23
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
EDAC MC: Ver: 3.0.0
Switched to clocksource timebase
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 2900K (efd2a000 - effff000)
Freescale PMC driver
audit: initializing netlink socket (disabled)
type=2000 audit(0.188:1): initialized
bounce pool size: 64 pages
HugeTLB registered 1 MB page size, pre-allocated 0 pages
HugeTLB registered 4 MB page size, pre-allocated 0 pages
HugeTLB registered 16 MB page size, pre-allocated 0 pages
HugeTLB registered 64 MB page size, pre-allocated 0 pages
HugeTLB registered 256 MB page size, pre-allocated 0 pages
HugeTLB registered 1 GB page size, pre-allocated 0 pages
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
NTFS driver 2.1.30 [Flags: R/O].
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 1502
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 2 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0xd8004500 (irq = 42, base_baud = 25000000) is a 16550A
console [ttyS0] enabled, bootconsole disabled
console [ttyS0] enabled, bootconsole disabled
Generic non-volatile memory driver v1.1
brd: module loaded
loop: module loaded
nbd: registered device at major 43
Uniform Multi-Platform E-IDE driver
ide-gd driver 1.18
st: Version 20101219, fixed bufsize 32768, s/g segs 256
fsl-sata d8018000.sata: Sata FSL Platform/CSB Driver init
scsi0 : sata_fsl
ata1: SATA max UDMA/133 irq 74
fsl-sata d8019000.sata: Sata FSL Platform/CSB Driver init
scsi1 : sata_fsl
ata2: SATA max UDMA/133 irq 41
fe000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000001 Chip ID 0x002801
NOR chip too large to fit in mapping. Attempting to cope...
Amd/Fujitsu Extended Query Table at 0x0040
Amd/Fujitsu Extended Query version 1.3.
number of CFI chips: 1
Reducing visibility of 131072KiB chip to 32768KiB
4 ofpart partitions found on MTD device fe000000.nor
Creating 4 MTD partitions on "fe000000.nor":
0x000000040000-0x000000080000 : "NOR DTB Image"
0x000000080000-0x000000780000 : "NOR Linux Kernel Image"
0x000000800000-0x000001c00000 : "NOR JFFS2 Root File System"
0x000001ec0000-0x000002000000 : "NOR U-Boot Image"
fsl_espi d8007000.spi: master is unqueued, this is deprecated
m25p80 spi32766.0: unrecognized JEDEC id ffffff
fsl_espi d8007000.spi: chipselect 0 already in use
spi_master spi32766: spi_device register error /soc@d8000000/spi@7000/slic@0
fsl_espi d8007000.spi: at 0xf1082000 (irq = 59)
libphy: Fixed MDIO Bus: probed
libphy: Freescale PowerQUICC MII Bus: probed
mdio_bus mdio@d8024000: cannot get PHY at address 1
mdio_bus mdio@d8024000: cannot get PHY at address 0
mdio_bus mdio@d8024000: cannot get PHY at address 2
mdio_bus mdio@d8024000: cannot get PHY at address 3
libphy: Freescale PowerQUICC MII Bus: probed
libphy: Freescale PowerQUICC MII Bus: probed
fsl-gianfar ethernet.2: enabled errata workarounds, flags: 0x4
fsl-gianfar ethernet.2 eth0: mac: 00:00:00:00:00:00
fsl-gianfar ethernet.2 eth0: Running with NAPI enabled
fsl-gianfar ethernet.2 eth0: RX BD ring size for Q[0]: 256
fsl-gianfar ethernet.2 eth0: TX BD ring size for Q[0]: 256
fsl-gianfar ethernet.3: enabled errata workarounds, flags: 0x4
fsl-gianfar ethernet.3 eth1: mac: 00:00:00:00:00:00
fsl-gianfar ethernet.3 eth1: Running with NAPI enabled
fsl-gianfar ethernet.3 eth1: RX BD ring size for Q[0]: 256
fsl-gianfar ethernet.3 eth1: TX BD ring size for Q[0]: 256
fsl-gianfar ethernet.4: enabled errata workarounds, flags: 0x4
fsl-gianfar ethernet.4 eth2: mac: 00:00:00:00:00:00
fsl-gianfar ethernet.4 eth2: Running with NAPI enabled
fsl-gianfar ethernet.4 eth2: RX BD ring size for Q[0]: 256
fsl-gianfar ethernet.4 eth2: TX BD ring size for Q[0]: 256
pps pps0: new PPS source ptp0
ucc_geth_driver: QE UCC Gigabit Ethernet Controller
e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
e1000: Copyright (c) 1999-2006 Intel Corporation.
e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
e1000e: Copyright(c) 1999 - 2013 Intel Corporation.
igb: Intel(R) Gigabit Ethernet Network Driver - version 5.0.5-k
igb: Copyright (c) 2007-2013 Intel Corporation.
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci-pci: OHCI PCI platform driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 28, io mem 0xd8022000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new interface driver usb-storage
rtc-test rtc-test.0: rtc core: registered test as rtc0
rtc-test rtc-test.1: rtc core: registered test as rtc1
i2c /dev entries driver
mpc-i2c d8003000.i2c: timeout 1000000 us
mpc-i2c d8003100.i2c: timeout 1000000 us
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
caam d8030000.crypto: device ID = 0x0a14010000000000 (Era 3)
caam d8030000.crypto: job rings = 4, qi = 0
caam_jr d8031000.jr: failed to flush job ring 0
caam_jr: probe of d8031000.jr failed with error -5
caam_jr d8032000.jr: failed to flush job ring 1
caam_jr: probe of d8032000.jr failed with error -5
caam_jr d8033000.jr: failed to flush job ring 2
caam_jr: probe of d8033000.jr failed with error -5
caam_jr d8034000.jr: failed to flush job ring 3
caam_jr: probe of d8034000.jr failed with error -5
caam algorithms registered in /proc/crypto
Job Ring Device allocation for transform failed
caam d8030000.crypto: fsl,sec-v4.4 algorithms registered in /proc/crypto
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ipip: IPv4 over IPv4 tunneling driver
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
Key type dns_resolver registered
rtc-test rtc-test.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
ata1: No Device OR PHYRDY change,Hstatus = 0xa0000000
ata1: SATA link down (SStatus 0 SControl 300)
ata2: No Device OR PHYRDY change,Hstatus = 0xa0000000
ata2: SATA link down (SStatus 0 SControl 300)
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing unused kernel memory: 228K (c0724000 - c075d000)
INIT: version 2.88 booting
Starting udev
udevd[1343]: starting version 182
Starting Bootlog daemon: bootlogd.
Populating dev cache
Thu Sep 29 12:48:00 UTC 2016
rtc-test rtc-test.0: test_rtc_set_mmss, secs = 1475153280
Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...
update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)
INIT: Entering runlevel: 5
Configuring network interfaces... done.
Starting syslogd/klogd: done
Stopping Bootlog daemon: bootlogd.
What can I do now? I think the linux image and the file system have already started!I have hang here for a long time, please help me!
Respect for your reply, thank you!