CW10.5.1 connection failed,ccs config string is invaild(ccsprotocolplugin)!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.5.1 connection failed,ccs config string is invaild(ccsprotocolplugin)!!

1,275件の閲覧回数
longqiluo
Contributor II

hello, I just want use CW10.5.1 ev and Codewarrior  TAP(over USB) for write bootloader to P1023 norflash,S29GL512P,my connection configuration like below:

pastedImage_0.png

pastedImage_1.pngbut when I erase flash there is always say ,Connection failed,ccs config string is invalid,like the pictrue:pastedImage_2.pnganyone can help me ??

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,162件の閲覧回数
Pavel
NXP Employee
NXP Employee

Check connection to CodeWarrior TAP using CodeWarrior TAP User Guide:

http://www.nxp.com/files/soft_dev_tools/doc/user_guide/CWTAPUG.pdf?fasp=1&WT_TYPE=Users%20Guides&WT_...

Is there CodeWarrior TAP in Device Manager? See attached screenshot.

Is there connection to CodeWarrior TAP configuration console? See the Section 2.2.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,162件の閲覧回数
longqiluo
Contributor II

thank your apply!! I think I got little progress ,but I programmer flash there is still a wrong like below,any suggestions?

pastedImage_0.png

0 件の賞賛
返信