COP/JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

COP/JTAG

3,043件の閲覧回数
tomaszkrupski
Contributor I

Hi!

Is it possible to use a COP connector (J29 in the P1010RDB)  for the boundary scan test?

In my design a JTAG chain consist of a CPLD, P1010, and FPGA.

Will a debugging of  P1010 through COP still work, even when the P1010 is in the middle of a JTAG chain?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,288件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tomasz,

It is possible to debug P1010 in the JTAG chain.

First please make sure TDI and TDO of the JTAG header and all the devices in the chain are connected.

If you use CodeWarrior, you need to define JTAG configuration file for the scan chain.

The CodeWarrior debugger  supports targets with non-Freescale devices on the scan

chain. Each non-Freescale device is declared as "generic" and needs three parameters:

JTAG Instruction Length; Bypass Command; and Bypass Length. The values for these

three parameters are available in the device's data sheet or from its manufacturer.

For example, the JTAG Configuration File for this scan chain could be as the following.

Generic 4 1 0xF

P1010

Generic 5 1 0x1F


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,288件の閲覧回数
lunminliang
NXP Employee
NXP Employee

I thinks yes, what's your problem?

See Section 8.3 Using JTAG Configuration File to Specify Multiple Linked Devices on a JTAG Chain, in Targeting_PA_Processors.pdf, the document is located in the CW installation C:\Freescale\CW_PA_v10.3.3\PA\Help\PDF.

0 件の賞賛
返信