Advertised e5500 dhrystone MIPs/MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Advertised e5500 dhrystone MIPs/MHz

2,332件の閲覧回数
deans
Contributor I

NXP advertises 3 MIPs/MHz - what toolchain and options were used to achieve this performance?

Thanks,

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,019件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Originally they use GCC 4.5.1 compiler and compile Dhrystone version V2.1 with optimization level O2. If you need more details please create technical case - refer the following link:

https://community.freescale.com/thread/381898

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,019件の閲覧回数
deans
Contributor I

I am only getting 1.8 MIPs/MHz on a P5020DS using GCC 4.7.2 (CodeWarrior) w/ -O3.

I will open a support request.

0 件の賞賛
返信