Adjust the DDR refresh interval

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adjust the DDR refresh interval

2,506件の閲覧回数
ivanzhang
Contributor II

Can I adjust the register DDR_SDRAM_INTERVAL of P2020 after the MEM_EN bit of the register DDR_SDRAM_CFG has been setted ?

If it can't be realized, how can I adjust the refresh interval when the DDR controller is working ?

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,290件の閲覧回数
ufedor
NXP Employee
NXP Employee

During normal DDR controller operation it is not required to change its registers values, so the controller behaviour is not specified/guaranteed after a register value is changed when MEM_EN=1.

0 件の賞賛
返信

2,290件の閲覧回数
ivanzhang
Contributor II

When Tcase of DDR is over 105℃, I need to change the refresh interval, so how to realize?

0 件の賞賛
返信

2,290件の閲覧回数
ufedor
NXP Employee
NXP Employee

Use higher refresh rate from the very beginning.

0 件の賞賛
返信