Adjust the DDR refresh interval

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adjust the DDR refresh interval

2,517 次查看
ivanzhang
Contributor II

Can I adjust the register DDR_SDRAM_INTERVAL of P2020 after the MEM_EN bit of the register DDR_SDRAM_CFG has been setted ?

If it can't be realized, how can I adjust the refresh interval when the DDR controller is working ?

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

2,301 次查看
ufedor
NXP Employee
NXP Employee

During normal DDR controller operation it is not required to change its registers values, so the controller behaviour is not specified/guaranteed after a register value is changed when MEM_EN=1.

0 项奖励
回复

2,301 次查看
ivanzhang
Contributor II

When Tcase of DDR is over 105℃, I need to change the refresh interval, so how to realize?

0 项奖励
回复

2,301 次查看
ufedor
NXP Employee
NXP Employee

Use higher refresh rate from the very beginning.

0 项奖励
回复