Active driven voltage level for VBUSCLMP on P1010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Active driven voltage level for VBUSCLMP on P1010

2,024 Views
davef
Contributor I

The P1010 datasheet states that VBUSCLMP is in the 3.3V pin group, but the reference design drives the pin to about 1.3V via a resistor-divided VBUS.

What is the correct voltage to drive this pin to assuming we are using the PHY, but not generating VBUS (internal mPCIE USB interface).

Thanks...

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

1,769 Views
davef
Contributor I

Bump.

0 Kudos
Reply

1,769 Views
Pavel
NXP Employee
NXP Employee

Sorry for delay.

The VBUSCLMP circuit power supply is 3.3V. The VBUSCLMP absolute maximum rating is –0.3V to 3.63V.

Factory recommends using external divider to reduce the voltage range into 0v to 1.37V.

0 Kudos
Reply

1,769 Views
Pavel
NXP Employee
NXP Employee

The P1010 USB controller uses VBUSCLP input as input for detection VBUS voltage.

The P1010 USB controller hardware provides correct working if voltage on this pin is in range into 0v to 1.37V.

Therefore external voltage divider in Vbus usually is used to reduce the voltage range into 0v to 1.37V (external vbus divider ratio is 0.2626).

Factory recommends using divider with precise 51.1k / 18.2k.

This divider is needed if the P1010 USB PHY is not used.

0 Kudos
Reply

1,769 Views
davef
Contributor I

As I stated above, we aren't generating VBUS, so we can't use that specific voltage divider.

Is there a spec for Vin-low(max) and Vin-high(min) for the VBUSCLMP pin? And what is the absolute max voltage we can drive the pin to?

0 Kudos
Reply