P1020/P1011 Reset Configuration Specific FAQs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1020/P1011 Reset Configuration Specific FAQs

P1020/P1011 Reset Configuration Specific FAQs

Should I tie "UART_RTS_B01" to "0" while configuring signals sampled at reset in P1011?

If eTSEC1 is required in RGMII mode then the POR configuration pins should be set to {EC_MDC,TSEC1_TXD0,TSEC1_TXD7} = {010} and if eTSEC3 is required in RGMII mode then {UART_RTS0,UART_RTS1,TSEC_1588_ALARM_OUT2} = {101}

As all above signals default POR value is 1, you have to specify the signals that should be externally pull-down through a resistor when ever logic zero is required


ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎07-25-2012 10:46 AM
更新者: