P1020/P1011 Reset Configuration Specific FAQs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1020/P1011 Reset Configuration Specific FAQs

P1020/P1011 Reset Configuration Specific FAQs

Should I tie "UART_RTS_B01" to "0" while configuring signals sampled at reset in P1011?

If eTSEC1 is required in RGMII mode then the POR configuration pins should be set to {EC_MDC,TSEC1_TXD0,TSEC1_TXD7} = {010} and if eTSEC3 is required in RGMII mode then {UART_RTS0,UART_RTS1,TSEC_1588_ALARM_OUT2} = {101}

As all above signals default POR value is 1, you have to specify the signals that should be externally pull-down through a resistor when ever logic zero is required


标签 (1)
无评分
版本历史
最后更新:
‎07-25-2012 10:46 AM
更新人: