Hello,
isolation: yes
current on the second side: max 1A
Von: guoweisun
Gesendet: Donnerstag, 22. März 2018 02:54
An: Binder Christian
Betreff: Re: - Re: using the TEA1833 for a DC-DC converter
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: using the TEA1833 for a DC-DC converter
reply from G.w. Sun<https://community.nxp.com/people/guoweisun?et=watches.email.thread> in Other NXP Solutions - View the full discussion<https://community.nxp.com/message/998148?commentID=998148&et=watches.email.thread#comment-998148>