using the TEA1833 for a DC-DC converter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using the TEA1833 for a DC-DC converter

1,059 Views
christianbinder
Contributor I

can I use the TEA1833 for a DC-DC converter? Vin: 60-160VDC; V-Output: 45VDC

0 Kudos
Reply
3 Replies

1,000 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

I think you can use it!

Normally we will design the VIN minimum 60VAC,you can modify the brown in/out circuit to meet your request 60VDC input.

0 Kudos
Reply

1,000 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

What is output current? Do you need  isolation between primary and second side?

0 Kudos
Reply

1,000 Views
christianbinder
Contributor I

Hello,

isolation: yes

current on the second side: max 1A

Von: guoweisun

Gesendet: Donnerstag, 22. März 2018 02:54

An: Binder Christian

Betreff: Re: - Re: using the TEA1833 for a DC-DC converter

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: using the TEA1833 for a DC-DC converter

reply from G.w. Sun<https://community.nxp.com/people/guoweisun?et=watches.email.thread> in Other NXP Solutions - View the full discussion<https://community.nxp.com/message/998148?commentID=998148&et=watches.email.thread#comment-998148>

0 Kudos
Reply